STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

When stepping through code the debug window gets the focus momentarily after each step, and then back to the main.c window. I don't remember this happening. Anyway to turn this off ?

I am using STM32CubeIDE on linux Also an aside the debugger is having problems finding source files even if I give it the correct {project}/Core/Src directory. When I give it the actual file it is happy. Thank you and have a productive day : )

stm32f103 USB hid library is not very useful

Im on that new CubeIDE, all updated. My MCU is f103.Making hid device, which should have a few reports, more than 1. So, i edited report descriptor, added reportID, added second report. Windows recognizes it just fine.But what a surprise, second repo...

VLuky by Associate II
  • 1145 Views
  • 0 replies
  • 0 kudos

Projects not building after update

Hi, today I updated CubeIDE to version 1.3.1 and my working projects and also newly generated projects won't build. I'm getting 114 error messeges of this type: "Error: selected processor does not support `dsb ' in Thumb mode". Also in project settin...

ANiko.2 by Associate
  • 1200 Views
  • 1 replies
  • 0 kudos

Build multiple binary files in 1 project

Hello there :I want to build multiple bin files with specific address and length in CubeIDE/Eclipse,for example , I have my linker file like :MEMORY:{ SYSTEM_BIN(wr) :ORIGIN = 0x8008800 ,LENGTH = 8K PCU_BIN(wr) :ORIGIN = 0x800A800 ,LENGTH = ...

WYang.2 by Associate
  • 2457 Views
  • 3 replies
  • 1 kudos

Resolved! DMA IRQ Handler is called twice for ADC

Hi,I am using 3 ADC modules triggered with TIM3 to start in the same time.I read the result in the DMAx_Channely_IRQHandler function and for debug only I do a toggle in a GPIO.I have 3 DMAx_Channely_IRQHandler functions , one for each ADC with DMA an...

DKuro.1 by Associate III
  • 2004 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.