STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32CubeIDE Disassembly Error

Hello,i use STM32CubeIDE to program STM32H753 and i now got this error in my disassembly (attached).The Code Piece is attached too.I tried a bit and have seen that the error only occurs when i add the for-loop. Without it, its all ok. When i move the...

Resolved! STM32F769I-Disco Blinky: Debugger Connection Lost

I keep getting the following failures when I try to run/debug a simple blinky program on my dev board. This is a fresh install of stm32cubeide, new project started with all peripherals NOT set to default settings. Instead I just set pin N3 (GPIOA, Pi...

MMiri.1 by Associate II
  • 1982 Views
  • 4 replies
  • 1 kudos

Resolved! Error when i try to update STM32

Hello,When i try to update STM32, it's give an error and it doesn't update. An error occurred while collecting items to be installedsession context was:(profile=STM32CubeIDE, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=, acti...

MDrei.1 by Associate
  • 4573 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.