2020-03-27 2:42 PM
Hi,
I am using STM32CubeIDE 1.3.0 on Linux Debian, and when I try to flash the MCU using the Run Button, GDB fails with error "bind failed. Error = 98, exit" (it seems that the IDE is trying to open an busy connection).
Concretely the log from console is the following:
STMicroelectronics ST-LINK GDB server. Version 5.5.0
Copyright (c) 2019, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Info : default port : 7184
Info : Remote address: 127.0.0.1
Error: bind failed. Error = 98, exit
Waiting for debugger connection...
Debugger connected
-------------------------------------------------------------------
STM32CubeProgrammer v2.4.0
-------------------------------------------------------------------
ST-Link Server is running on port : 7184
Info : default port : 7184
Info : Remote address: 127.0.0.1
Error: bind failed. Error = 98, exit
Info : default port : 7184
Info : Remote address: 127.0.0.1
Error: bind failed. Error = 98, exit
ST-LINK SN : 56FF70067878545228080567
ST-LINK FW : V2J36S7
Voltage : 3.05V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x413
Device name : STM32F405xx/F407xx/F415xx/F417xx
Flash size : 1 MBytes (default)
Device type : MCU
Device CPU : Cortex-M4
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_S0Km9U.srec
File : ST-LINK_GDB_server_S0Km9U.srec
Size : 6932 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sector 0
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:00.566
Verifying ...
Download verified successfully
Info : default port : 7184
Info : Remote address: 127.0.0.1
Error: bind failed. Error = 98, exit
Debugger connection lost.
Shutting down...
Do I have a wrong environment configuration ?
Otherwise, is it a known bug ?
Thanks for any suggestion.
s.
2020-05-06 3:59 AM
I encountered this error message, and I debugged it with the following command:
$ sudo lsof | grep 'TCP.*7184'
stlink-se 4555 mt 3u IPv4 20724358 0t0 TCP localhost:7184 (LISTEN)
stlink-se 4555 4558 mt 3u IPv4 20724358 0t0 TCP localhost:7184 (LISTEN)This reveals there's already an instance of stlink-server running, it's process ID 4555, and it's bound to TCP port 7184 - checking with ps fax revealed stlink-server had already been started by stm32cubeide
I ran killall stlink-server to remove the old instance.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.