STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Is STM32CubeIDE compatible with SPL Library?

Hi Every I am new to this platform.​my question is as the topic stated above. My situation is that I have my completed project on Keil Vision 5 which works well, but for some reason I need to migrate the whole firmware to STM32CubeIDE. ​I googled abo...

0693W000001ceJmQAI.png
WAi.11 by Associate II
  • 5013 Views
  • 7 replies
  • 0 kudos

STM32F746G-Discovery ADC3 refuses to trigger off TMR5 (any timer) using default cubemx prj config in STM32CubeIDE Version: 1.3.1. The interrupt from T5 works. ADC works when soft-start. Is this an ADC3 issue? Can I use SWD/trace to see ADC status? How?

static void MX_ADC3_Init(void){ ADC_ChannelConfTypeDef sConfig = {0};... hadc3.Instance = ADC3; hadc3.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV4; hadc3.Init.Resolution = ADC_RESOLUTION_12B; hadc3.Init.ScanConvMode = ADC_SCAN_ENABLE; hadc3.Init.Co...

SStep.11 by Associate II
  • 2069 Views
  • 4 replies
  • 0 kudos

Problem with HRTIM with Nucleo-H743ZI2 Board

Hello Everybody I have the Problem with my Hightimer PWM Output. If I define that my HRTIM is working with 480MHz (CPU_Ck). it will not and work with the normal 240MHz Output.Why is that so?

PVZ by Associate II
  • 4236 Views
  • 6 replies
  • 0 kudos

Resolved! Nucleo-G431KB help with DMA GPIO Output

Hi there!I've just started working with STM32CubeIDE and after a bit of a vertical learning curve I'm slowly getting to grips with most aspects of it.I want to DMA to GPIO and there doesn't appear to be any way to do this through the .ioc GUI interfa...

etheory by Senior II
  • 9212 Views
  • 24 replies
  • 0 kudos

Resolved! STM32CubeIde techniques ?

I want to know how to fold curly braces. There are too many codes in the interface, so i hope the brace can be folded.

Xli.1 by Associate
  • 3230 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.