STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Stm32Cube IDE character spacing not consistent

Running STM32CubeIDE versions 1.18.1 and 1.19.0istatic char *Audio3D[] = { // Main Settings display"THERE ARE 15 VOLUME ",IDE version 1.18.1 displays a 21 character line of code with the quotes one ontop of the other.static char *Temp2D[] = { " TEMPE...

JBonn by Associate III
  • 658 Views
  • 4 replies
  • 2 kudos

Trace buffer is full - using the SWV viewer

Hello, I am using the SWV viewer successfully to output messages from the microcontroller at runtime. This is a nice tool and usually it works fine.  When I run an application for a longer time (e.g. over night) I get this errorI did consider the tra...

2025-08-11 07_24_40-workspace - TST_SGP41_Drivers_SGP41_API_STM32_SGP41.cpp - STM32CubeIDE.png
DocAlex by Associate III
  • 882 Views
  • 4 replies
  • 0 kudos

STM32CubeIDE 1.19.0 live expression fail

Hi everyone,STM32CubeIDE v 1.19.0MCU: stm32h755I am debugging correctly the dueal core by means i see all registers in the live expression changing values without my intervention as expected by the simple code i wrote. As soon as i input a value, let...

Zzaaack_0-1755159145039.png
Zzaaack by Associate III
  • 995 Views
  • 3 replies
  • 0 kudos

X CUBE AI

After model analysis is performed on the model complexity using X-CUBE AI import, the code will be generated.Unknown type name 'ai_i8'Unknown type name 'ai_handle'Creation Failed. I'm getting 19 errors.Has anyone else encountered this? I think an upd...

Resolved! Switching STM32C011F4U6TR to STM32C071G8U6 - many errors

HiI am trying to switch a project from one MCU to the another. I made a new IOC file in MX and then replaced the existing IOC file in my IDE project with my fresh file. The overall configuration is identical except for the pinout, and I use a mix of ...

kzsd by Associate II
  • 1815 Views
  • 10 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.