STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Bug in STM32CubeIDE v1.3.0 - tick mark and radio button not getting selected for SWV

We have a issue with STM32CubeIDE v1.3.0 - this version is an update form our previous bug report "Security Issue - installation on Ubuntu changes the owner:group of /etc"Reproducible: yesOS: Ubuntu 20.04ST software: STM32CubeIDE v1.3.0 with patch f...

Transfer code from IAR to CubeIDE?

HiI have been requested to redesign a current product using an ST32F405RG where the software was developed in the IAR IDE.This is mainly a HW update that requires only a little bit of SW changes.Unfortunately the IAR IDE is not available. Hence, I wo...

TNils.1 by Associate II
  • 2822 Views
  • 3 replies
  • 0 kudos

Resolved! STM32F411EDISCO - USB Device example

Hi I bought STM32F411E DISCO board for project and want to develop a custom USB Device for communication with PC I need some information on following How to use STM32CUBE software (IDE, Complier) with this board Where is Embedded software and librari...

DHinge by Associate II
  • 3278 Views
  • 5 replies
  • 0 kudos

Resolved! STM32CubeIDE can't use gmp.h?

I wanna use big number in my board.So, i try to use 'gmp.h'.But when i use 'mpz_init' function, that have error message like this. -> 'undefined reference to `__gmpz_init''​Should I make this function myself????

HYoun by Associate II
  • 5464 Views
  • 3 replies
  • 0 kudos

Unable to get a valid ADC-value

Hello everyone,at first the Discoveryboard I'm using is the P-L496G-Cell02 / STM32L496G-DISC.To test the ADC I tried to recieve a value from a potentiometer. So I started a new STM32CuvbeIDE project, Selected the board I'm using and changed the Pins ...

FEich.1 by Associate II
  • 6124 Views
  • 11 replies
  • 0 kudos

Resolved! STM32CubeIDE Not Responding after update

I recently updated my IDE, and when trying to open my project I get the expected "Project has been created with 5.6.1 and needs to be updated", but whether I click "Migrate" or "Continue", the whole IDE just goes to "not responding" and I have to clo...

0693W000003Q36GQAS.png
GearHead by Associate II
  • 1706 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.