2020-08-12 3:45 AM
Hi
I have been requested to redesign a current product using an ST32F405RG where the software was developed in the IAR IDE.
This is mainly a HW update that requires only a little bit of SW changes.
Unfortunately the IAR IDE is not available. Hence, I wonder if it is possible/feasible to use/transfer the code/files from the IAR environment and use them in ST's CubeIDE?
If possible, how cumbersome can I expect it to be?
Thanks!
2020-08-12 5:43 AM
> If possible, how cumbersome can I expect it to be?
It should be quite manageable.
2020-08-12 6:47 AM
Great, thanks!
2020-08-25 6:06 AM
If it hadn't been for the great mess in the original files, migrating via Atollic Truestudio made it very manageable ;)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.