STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

[NOT Solved] F407 and SanDisk Cruzer Blade 16GB don't work (32GB work)

I tested 3 pendrives, 4GB (Samsung?), 16GB and 32GB (SanDisk Cruzer Blade).​Two worked on the STM32F407VG.​SD card adapter also doesn't work, 8GB (Kingston), 2GB (Generic), 16GB (Sandisk Ultra).​SanDisk Cruzer Blade 16GB don't work.​Using USB host wi...

by Not applicable
  • 8084 Views
  • 19 replies
  • 0 kudos

UART4_RX and UART5_RX requests were not downloaded

HI everyone,Sorry I am not familiar with STM32Cube IDE.After I created a workspace for my project, I encountered an warning message that says "UART4_RX and UART5_RX and UART4_TX and UART5_TX_DMA requests were not loaded."If I encountered this, what i...

0693W000003PvYCQA0.png
DSant.1 by Associate
  • 1441 Views
  • 2 replies
  • 0 kudos

When I create a new stm32project and I try to debug it, STM32CUBEide give me the follow message: "Break at address "0xfffffffe" with no debug information available, or outside of program code." What I can do?

I've found in a forum the follow indication:"The address is outside of any allowed code addresses in a Cortex-M4. The code has probably tried to use unprogrammed flash (0xffffffff) as a return address, see the contents of the link register (R14)."How...

FSvig.1 by Associate
  • 1150 Views
  • 1 replies
  • 0 kudos

Why '.bss' was created in both Flash and RAM? This causes "section `.bss' will not fit in region `RAM'" in my application.

Hi All,I have created a STM32 application using STM32CUBDEIDE. I'm using STM32F469IH6 for this project.I have declared few uninitialized variables in one file. I know this affects ".bss" section but it is required in my code. This causes an error say...

0693W000003PtXMQA0.png
HNall.1 by Associate III
  • 7545 Views
  • 8 replies
  • 0 kudos

Resolved! Use second firmware as function, called when necessary

Hi!I want to use 2 firmware on the same microcontroller, one is written at 0x8000000 with ram starting at 0x20000000. The other is flashed at 0x8040000 with ram starting at 0x20010000.The first firmware should use the second as a function. So i alloc...

LSpad.1 by Associate III
  • 2028 Views
  • 3 replies
  • 0 kudos

STM32 OTA? Goodbye to ST-Link? How to upload via internet?

I found a project that allows the programming of STM32 via OTA, it would be very interesting if the STM32CubeIDE could work directly with this.[STM32 OTA using esp8266]:https://www.youtube.com/watch?v=aqYHebO789UDoes anyone know if it is possible to ...

by Not applicable
  • 2279 Views
  • 2 replies
  • 1 kudos

Resolved! In STM32CubeIDE, can I add python script to auto-run before compiler runs? To increment a BUILD number in *.H file.

In old AC6 workbench, I could add such python script as external tool to auto-build always before compiler runs. Now with STM32CubeIDE, I've found how to do manually with 'external tools' button. Can I add back to project to auto-run again?

Resolved! edit makefile

HelloI am using stm32Cube IDE.Where should I edit the makefile?Thank you.

Ebun.1 by Senior
  • 3568 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.