STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32CubeIDE, unable to program and debug on Windows 7

Using STM32CubeIDE version 1.4.2 on a Windows 7 64-Bit Home Premium Edition, Version 6.1 (Build 7600) laptop, I am unable to program and debug a project on a NUCLEO-F401RE board.When I attempt to debug to program the board and debug and run the firmw...

0693W000003RdXUQA0.png 0693W000003RdUuQAK.png 0693W000003RdWCQA0.png
dlkeng by Associate III
  • 1272 Views
  • 0 replies
  • 0 kudos

Resolved! How to get ARM semihosting to work on STM32CubeIDE

I just started using STM32CubeIDE, and was able to get a blinking LED and getting some UART communication going in no time with a NUCLEO-L476RG eval board.I am trying to follow the examples in the book "Mastering STM32" by Carmine Noviello, but I am ...

MGoss.2 by Associate
  • 9037 Views
  • 6 replies
  • 0 kudos

Error : unknown type name 'class'

Hello,I am migrating from Arduino to CubeIDE looking to have better IDE and better performance code. Migration was rather challenging but managed to go ahead. Still there is one new issue I have.I created a C++ project using CubeMX but I get this err...

CSand by Associate III
  • 13458 Views
  • 1 replies
  • 2 kudos

Resolved! STM32F407VG Led Blink Button Problem

Hello, i'm a new about this embedded systems, i am working with stm32f4 discovery card with HAL Library.İ looked the GPİO topic and i want to create a program like :When i clikt the button 3 times red led will open and when i clikc the button 5 times...

0693W000003RUfeQAG.png 0693W000003RUtMQAW.png

Stop console output for Live Expressions

Hello,Using LiveExpressions produces a large amount of unwanted console output like "Reading x bytes @ address 0xxxxxxxxx".Is it possible to disable such console output when not needed?Thank you in advance.

Resolved! Triggering ADC/DMA with Timer2 (STM32WB55)

Hello! I had a project where I'm trying to get the ADC/DMA to trigger with timer 2 but I seem to be missing part of the puzzle to getting it up and working. I originally had the ADC/DMA running with "Continuous Conversion" mode set in the ADC, which ...

0693W000003RMCZQA4.jpg 0693W000003RMCUQA4.jpg 0693W000003RMCAQA4.jpg 0693W000003RMC0QAO.jpg
JayDev by Senior II
  • 2121 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.