STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! STM32U5 UCPD PDO Num BUGs

Board:STM32U5A9xxI set the Number of PDO to define = 5 in the cubeide.But after generate code, the code in usbpd_pdo_defs.h, macro:PORT0_NB_SINKPDO is still 1U.I also checked the file usbpd_pdo_defs_u5.ftl in cubeide's location, the macro PORT0_NB_SI...

Jason927_0-1756195540325.png
Jason927 by Associate III
  • 979 Views
  • 5 replies
  • 1 kudos

SYS_DBG_ENABLE_TA4 BUG IN v 1.19.0

Working with getting TraceRecorder to work with an L562 project.  When the tracerecorder software is added (using the package), SYS_DBG_ENABLE_TA4 is set to 0, which inactivates the feature.  SYS_DBG_ENABLE_TA4 has to be manually set to 1 to enable t...

Resolved! STM32 NUCLEO H755ZIQ USART bug

  I have been trying to deploy a simple ML model on my STM32 NUCLEO H755ZIQ, i've been following a tutorial as am learning right now, but no matter how many times i try i cant seem to shake of these three errors:1. when i try to open the XcubeAI  int...

Screenshot 2025-08-21 at 3.18.22 PM.png Screenshot 2025-08-21 at 3.46.29 PM.png vigneshn10_0-1755773483160.png

Resolved! STM32U5 Code Generation Bug?

Hi,i just generated a project using the Device Configuration Tool (1.19.0). All works. But as soon as I enable "Generate peripheral initialisation as a pair of '.c/.h' files per peripheral" the hardware stands at:static HAL_StatusTypeDef USB_CoreRese...

JE by Associate III
  • 1564 Views
  • 6 replies
  • 4 kudos

STM32CubeCLT 1.19.0 安装失败(Windows 系统),已尝试多种方案仍未解决

各位开发者好, 我在安装 STM32CubeCLT(版本:st-stm32cubeclt_1.19.0_25876_20250729_1159_x86_64.exe)时遇到问题,具体情况如下: 环境信息:作系统:Windows 10 64 位(版本 22H2)安装包来源:ST 官网下载安装路径:D:\STM32CubeCLT(纯英文,无特殊字符)问题现象:双击安装包无响应 / 弹窗报错(此前尝试图形化安装失败);尝试管理员身份运行 CMD,执行静默安装命令 ,命令行无明显报错,但安装目录未生成、...

_0-1755742850724.png
贰黑 by Associate
  • 1453 Views
  • 1 replies
  • 0 kudos

Resolved! IDE View and MX Generate

Hi, 1. I want ti have auto view change for C, MX and Debug windows. Previously a promt used to come. Now I dont see that.2. I want to generate MX automatic on save. Previously a promt used to come. Now I dont see that. 

GHK by Associate
  • 563 Views
  • 1 replies
  • 1 kudos

CubeIDE request

Hello,Dear ST,As a Big fan of yor MCU and everything based on eclipse please give possibility to disable in SFR view particular register or peripherals. Now without this possibility debugger can without my intention clears some flags (witch are clear...

Resolved! STM32CubeIDE Register View Problem

Hello EveryoneI am using the latest STM32CubeIDE i.e. 1.10.1, and I am facing a strange problem.In the register view of the Special Function Register, I have a problem.As can be seen above the RCC->CR register value is 0x30006783This means that Bit 2...

0693W00000VOHdqQAH.png 0693W00000VOHfDQAX.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.