2025-08-20 7:23 PM
2025-08-26 12:54 AM
Hello @贰黑
I used Reverso to translate your post.
I encountered an issue while installing STM32CubeCLT (version: st-stm32cubeclt_1.19.0_25876_20250729_1159_x86_64.exe). Here are the details:
Environment Information
Operating System: Windows 10 64-bit (version 22H2)
Installation Package Source: Downloaded from the official ST website
Installation Path: D:\STM32CubeCLT (English only, no special characters)
Problem Description
Double-clicking the installer does not produce any response or error message (previous attempts to run the installer also failed).
Running the installer from an elevated Command Prompt (as administrator) with the silent installation command does not show any errors, but no installation directory or key folders are created, confirming the installation failed.
Command used:
st-stm32cubeclt_1.19.0_25876_20250729_1159_x86_64.exe /Sbin
This is the first time installing this version, and any possible legacy files have been manually removed.
The installation package was verified using MD5 and is confirmed to be complete.
Actually I was capable to install the STM32CubeCLT (version: st-stm32cubeclt_1.19.0_25876_20250729_1159_x86_64.exe) on a windows10 machine which suggests that the issue may be specific to your environment.
To resolve the STM32CubeCLT installation issue, please try the following steps:
1- Check Windows Security Settings: Ensure the installer is not being blocked by Windows security settings or antivirus software.
2- Run as Administrator: Right-click the installer and select "Run as administrator."
3- Change Installation Directory: Try installing to a different directory (e.g., C:\STM32CubeCLT).
4- If you have access to another PC, try installing STM32CubeCLT there to see if the issue is specific to your current system.
THX
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.