STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

CubeIDE Execute command before debug

Hi,i would like to execute command after i click the debug icon, but before the debug starts.In particular:I have an app with a bootloader. The bootloader check the CRC of the firmware before start it.Right now i generate, thanks to post build operat...

LSpad.1 by Associate III
  • 3056 Views
  • 3 replies
  • 0 kudos

STM32CubeIde support C++17

I tried to find information on the internet, but I couldn't find anything. Replacing files in the plugins folder does not give the desired result. Is CubeIDE able to support C ++ 17?

AKlep.1 by Associate II
  • 1076 Views
  • 1 replies
  • 0 kudos

Resolved! Replace across all code files in project

Is there a way to do a Find/Replace across all the code files in a project or group of projects?i.e. change a variable name in a project or in all open projects?Paul

Paul1 by Lead
  • 4471 Views
  • 4 replies
  • 0 kudos

[BUG]Unable to run SWV on STM32F746 Nucleo board

Use STM32CubeIDE 1.4.2STM32CubeMX 6.0.1Windows 10 1903First of all generated ioc for truestudio 9.3. In main implement new _write function:int _write(int file, char *ptr, int len) { /* Implement your write code here, this is used by puts and printf f...

0693W0000059jflQAA.png 0693W0000059jgZQAQ.png 0693W0000059jkbQAA.png
GShch.1 by Associate
  • 912 Views
  • 0 replies
  • 0 kudos

Question about ioc file.

When modified the value of the ioc file, STM32CubeIDE creates the code.Conversely, if I modify the code, is there a way to reflect it in the ioc file?For example, if I change the PLLM value to 25 in the code, I want to automatically change the PLLM v...

SHong.4 by Associate
  • 810 Views
  • 1 replies
  • 0 kudos

Some issues with STM32CubeIDE and STM32H747

1) In all of the examples the project explorer shows the CM7 code greyed and crossed out because "exclude from build" is checked. It is clearly not excluded from the build as this is the main code for the example. I presume this is some fiddle to all...

AStew.1 by Associate II
  • 1336 Views
  • 2 replies
  • 0 kudos

Problem to add vl53l1 library

Hi, I have problem to add vl53l1 library to my project created whit STM32CUBE ide , i use mcu STM32G030FX, i unzip the file en.STSW-IMG007 under drivers/vl53l1/core and drivers/vl53l1/plattform ,after build the project i had this error16:37:31 ...

Fscu.1 by Associate II
  • 1178 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.