STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Set up External Memory in STM32CUBEIDE

Hi,i try to switch my working IDE from Atolic Truestudio to STM32CUBEIDE.A fraction of my code is executed on an external SDRAM.With Truestudio this works, when i initialize the SDRAM in a Startup Skript.I did't find the same feature in STM32CUBEIDE....

Minti by Associate II
  • 975 Views
  • 0 replies
  • 1 kudos

I have noticed that the HAL_I2C_Master_Transmit code is only sending write requests to even numbered addresses. A hardcoded address of 0x21 becomes 0x20 for instance.

I am trying to use an STM32-p405 to communicate with another device via I2C. The device has a number of potential addresses so I am sending commands to all of them to see which respond back. It wasn't working, and then I discovered none of the odd nu...

AMcAf.1 by Associate II
  • 3666 Views
  • 6 replies
  • 0 kudos

Resolved! I'm confused by the power consumption estimate in STM32CubeIDE

I'm starting a new STM32H7A3 project in STM32CubeIDE. I've got the peripherals assigned and would like to understand more precisely how each peripheral and things like CPU frequency affects current draw. When I first click on the Tools tab without...

magene by Senior II
  • 3452 Views
  • 5 replies
  • 0 kudos

C++ Support in STM32CubeIde - class symbol not accepted

Hello All,I made a C/C++ project with STM32CubeIde version 1.1.0. It works fine. Then I added a C++ class by a cpp and hpp file. And tried to make an instance of the class in the main.c file. The compiler does not recognize "class" symbol in my hpp f...

Jens1 by Associate
  • 5494 Views
  • 3 replies
  • 1 kudos

Resolved! Error "mode armelf" on GNU Tools for STM32 9-2020-q2-update

I have gotten a new error on a 1.5.0 that i have to seen anyware else before.Fresh install of 1.5.0Migrate 1.4.0 projectOpen project propertiesOpen Toolchain managerInstalll gnu tools for stm32 9-2020-q2-updaterestart cubeideSwitch to fixed selected ...

marbel by Associate II
  • 3301 Views
  • 6 replies
  • 0 kudos

Resolved! Missing LPTIMx_OR registers when debugging L452RETx

When I try and debug my program using CubeIDE 1.6.1 there are no LPTIMx_OR registers shown in the SFR LPTIMx register blocks. Am I doing something wrong or is this broken in the debugging environment? Using SMT32Cube MCU Package L4 1.17.0.TIA Pete

How to get 12 sec time using RTC

Hi ,I not used RTC earlier and new to RTC.I am using STM32L151RCT6 MCU and creating the project in STM32Cube IDE.what are the settings i need to do to get RTC timing of 12 sec..I searched and got some information about alarm time setting and alarm in...

MBhir.11 by Associate III
  • 2042 Views
  • 2 replies
  • 0 kudos

Issue with System Clock Configuration

I am trying to program an STM32 MCU powered board that has the STM32F103R8T6 UNIT. I have figured out that while the program is executing the function called SystemClock_Config(); doesn't initialize the clock and goes to the error handler when croosi...

TProt.1 by Associate II
  • 6424 Views
  • 4 replies
  • 0 kudos

New to Nucleo F429ZI + CubeIDE, easy tutorials needed

Hi,I haven't found tutorials for noobs like me yet.At first I'd like to blink my own 16 leds stripe through GPIOs using the CubeIDE.I only managed to tweak the .ioc pinout configuration and I can boot a code that lights up the leds connected to CN7 a...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.