2020-11-23 6:02 AM
I have gotten a new error on a 1.5.0 that i have to seen anyware else before.
Fresh install of 1.5.0
Migrate 1.4.0 project
Open project properties
Open Toolchain manager
Installl gnu tools for stm32 9-2020-q2-update
restart cubeide
Switch to fixed selected toolchain in settings and select the newly installed one
Apply and build
Get one error "mode armelf"
If i switch back to the other installed toolchain, it works fine.
(I do also btw get a waring about having assert redefined, but i hope that these issues are unrelated)
Best regards
Martin
Solved! Go to Solution.
2020-11-30 6:47 AM
Hi Martin,
There is no problem with the toolchain itself. It just seems to be a change with respect to log output when building with verbose flag.
gcc-7
==================================================
attempt to open c:/st/stm32cubeide_1.5.0/stm32cubeide/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.7-2018-q2-update.win32_1.5.0.202011040924/tools/bin/../lib/gcc/arm-none-eabi/7.3.1/thumb/v7e-m/fpv4-sp/hard/crti.o succeededgcc-9
==================================================
c:\st\stm32cubeide_1.5.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_1.5.0.202011040924\tools\arm-none-eabi\bin\ld.exe: mode armelf
attempt to open c:/st/stm32cubeide_1.5.0/stm32cubeide/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_1.5.0.202011040924/tools/bin/../lib/gcc/arm-none-eabi/9.3.1/thumb/v7e-m+fp/hard/crti.o succeededWith gcc.9 you get an additional log output (with verbose), see line 2 above. Linker is called in mode armelf. Nothing wrong here...
So why do you get an error in the "Problems view" and why is the line highlighted as red in the Console view?
This is because of the console error parser having a regexp that is not explicit enough.
So, if you want to get rid of the error you have two options:
Hope that solves the issue? Will fix for next version. Sharing the work-around here in case other users find the same issue.
Kind regards, Mattias
2020-11-24 7:56 AM
Hi,
We have not seen this issue before.
Kind regards, Mattias
2020-11-24 9:29 AM
Im on windows 10 on a x64 multicore.
Ill see if i can strip down the code tomorrow,
// Martin
2020-11-29 11:56 PM
I have sent you a DM
// Martin
2020-11-30 2:28 AM
Thanks - received the DM including the zip-file.
I can reproduce it on at least one win10 machine... Will get back with more info.
2020-11-30 6:47 AM
Hi Martin,
There is no problem with the toolchain itself. It just seems to be a change with respect to log output when building with verbose flag.
gcc-7
==================================================
attempt to open c:/st/stm32cubeide_1.5.0/stm32cubeide/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.7-2018-q2-update.win32_1.5.0.202011040924/tools/bin/../lib/gcc/arm-none-eabi/7.3.1/thumb/v7e-m/fpv4-sp/hard/crti.o succeededgcc-9
==================================================
c:\st\stm32cubeide_1.5.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_1.5.0.202011040924\tools\arm-none-eabi\bin\ld.exe: mode armelf
attempt to open c:/st/stm32cubeide_1.5.0/stm32cubeide/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_1.5.0.202011040924/tools/bin/../lib/gcc/arm-none-eabi/9.3.1/thumb/v7e-m+fp/hard/crti.o succeededWith gcc.9 you get an additional log output (with verbose), see line 2 above. Linker is called in mode armelf. Nothing wrong here...
So why do you get an error in the "Problems view" and why is the line highlighted as red in the Console view?
This is because of the console error parser having a regexp that is not explicit enough.
So, if you want to get rid of the error you have two options:
Hope that solves the issue? Will fix for next version. Sharing the work-around here in case other users find the same issue.
Kind regards, Mattias
2021-05-07 7:43 AM
This "linker error" wasted 3 of hours of my time!
This is issue still exists in version 1.6.1. Maybe it should be best for all of us to be included in next version.
Thank you so much Mattias.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.