STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

MPLAB features available in CubeIDE?

Hello.In MPLAB IDE there are two features that I find very helpful. (please see the attached file)Feature 1: Call GraphFeature 2: The code flow of where the cursor isAre any of these features available in CubeIDE?(Sorry I had to blacken things out, t...

mTiet.1 by Associate
  • 1908 Views
  • 2 replies
  • 0 kudos

Resolved! How to use USB CDC driver for STM32L053?

I've purchased an STM32L0358-disco board and I'm trying to get USB CDC to work. Here's the steps I took:Create a new project for the STM32L0538 mcu in STM32CubeIDEEnable the USB peripheralEnable the USB Middleware and set the class to Communication D...

JTeun.1 by Associate II
  • 5318 Views
  • 5 replies
  • 0 kudos

Issue when clone the project in STM32CubeIDE

Dear Sirs,I copy and pasted to clone the project in project explorer window of STM32CubeIDE.And some cases "Src" folder is automatically deleted from original project folder.:grinning_face_with_sweat: Does anyone faced similar issue ? and how can I ...

KKane by Associate II
  • 11858 Views
  • 22 replies
  • 1 kudos

STM32CubeIDE Linux Support

Hi,I'm trying to install STM32CubeIDE on Ubuntu 16.04. The release note of CubeIDE version 1.6.1 says it's tested on Ubuntu 18.04 and 20.04. Does v1.6.1 support Ubuntu 16.04? If not, which version of the IDE should I get?Thanks!

JLeng.2 by Associate
  • 1890 Views
  • 2 replies
  • 1 kudos

STM32CubeIDE and SWV ITM Data...once again. This is a bit long.

Looking for some clarification about printf and SWV ITM using an STM32F4-Discovery board (STM32F407VGT). Let's just assume we're working with boards/processors that support the function. What I have configured works but I'd like to understand this a ...

TJM by Senior II
  • 5693 Views
  • 7 replies
  • 0 kudos

How to Run/Debug "CMSIS-DSP" FFT examples in CubeIDE ?

Hello, I got an urgent problem. Anyone help me? Using Product : NUCLEO-H753ZI I have already setup the whole prepartion for using CMSIS-DSP library in my CubeIDE But It doesn't work and how to run the specific FFT example code ? <Done so far> Copy an...

0693W000004IlGIQA0.jpg
SBaik.1 by Associate
  • 2386 Views
  • 1 replies
  • 0 kudos

STEVAL-3DP 3D printer board...again...

Still trying to get the ST_Marlin firmware to compile under STM32CubeIDE and still unsuccessful. It just won't compile as copied OR migrated from SW4STM32 to the Cube. What I need is a step-by-step directory and file placement and configuration to ...

TJM by Senior II
  • 5017 Views
  • 16 replies
  • 0 kudos

Resolved! H757I - cannot use CM4 core

I have a STM32H757I eval board and I'm using STM32CubeIDE (last version), HAL v.1.8.0I've setup an empty project using the IDE.The problem is that the program for the CM7 core runs normally but as soon as i try to start the CM4 program everything "cr...

0693W000004IFEyQAO.png
NGior.1 by Associate
  • 2435 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.