STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! STM32Cube IDE app fails to run on latest macOS Monterey beta

I'm running the latest (less than one week old) macOS Monterey developer beta 12.4 (build 21F5063e) on a MacBook Pro 10,1 and downloaded the file en.st-stm32cubeide_1.9.0_12015_20220302_0855_x86_64.dmg_v1.9.0.zip, decompressed and installed the app. ...

0693W00000LzXVXQA3.png
mikew67 by Associate II
  • 2088 Views
  • 2 replies
  • 0 kudos

STM32CubeIDE 1.9.0 Question: User generated .c&.h files don't have the same functionality as the auto generated files like main.c.

I can add my own .ch files to a project and build and see the proper functionality on the MCU with no problems. However, the user generated src modules are not colorized, or system calls are not "Auto Complete" enabled like main.c module is. More imp...

FAssa.1 by Associate
  • 1203 Views
  • 3 replies
  • 0 kudos

Why SWD stopped working after re-programming?

I have an STM32G030 board that I was debugging, and all was going well. Then I started getting an 'unable to connect' message while debugging. Reading some of the forum, the issue appears to be that I checked "Set all free pins as analog (to optimize...

RLour.1 by Associate II
  • 5204 Views
  • 6 replies
  • 1 kudos

stm32 rx and tx interrupts interfere with each other

Hello,I am using STM32H743 Nucleo-144I have an RX EXTI interrupt which reads multiple SPI messages (a very busy channel)also, a TX interrupt which reads UDP messages dose small calculation and sends the new messages with SPI channel (pretty busy too)...

Mz.1 by Associate III
  • 2998 Views
  • 4 replies
  • 0 kudos

Cannot Copy a example Project in stm32cubeIDE

I'm trying to copy a project in cube IDE, version 1.9.0 windowsVery new to using stm32cubeIDE and Eclipse. So I'm hoping I've missed something fundamental, tried a couple of things but no success.I'm wanting to copy an example that st provide (BLE_p2...

Pcard.2 by Associate II
  • 3280 Views
  • 2 replies
  • 0 kudos

FAIL.txt file appears on the disk.

Once I connect my board(f746-disco), there is a disk in which FAIL.txt appears which contains "The interface firmware FAILED to reset/halt the target MCU". I have been getting this error since yesterday. I found a question asked this community, it wa...

My MCU (STM32H750B-DK) used to work normally but now the IDE shows error when I try to debug or communicate with it.

After using the MCU with no problem for weeks, i was trying to test a FDCAN application together with a raspberry pi, after that day, it's been having problems, it fails to connect to cube programmer, and it fails to run code that used to work perfec...

mhuar.1 by Associate II
  • 2331 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.