STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

(STM32F105C8, STM32CubeIDE 1.9.0, MacOS 11.6.5) Using STM32CubeIDE, how do I can't get TIM3 to tick/count when TIM2 overflows. (TIM2 does count up)

TIM2:Clock source: InternalMaster/Slave Mode: Disabled (Trigger input not delayed)Trigger Event Selection: Update EventTIM3:Slave Mode: Trigger ModeTrigger Source: ITR1TIM2 counts up like it should, but TIM3 doesn't count the over flow, but has incre...

FMoto.1 by Associate
  • 1743 Views
  • 2 replies
  • 1 kudos

Resolved! Failed to list external Loader

I try to add external loader to C:\ST\STM32CubeIDE_1.8.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.0.100.202110141430\tools\bin\ExternalLoaderIn debug configuration, check ExternalLodaer and than press Scan.Th...

ALomb.1 by Associate III
  • 9139 Views
  • 20 replies
  • 0 kudos
ltan.11 by Associate
  • 1858 Views
  • 1 replies
  • 0 kudos

Clicking on Search result opens the file in new Editor

Hi,This problem is observed in v1.9.0 as well as in earlier versions. If one clicks on any search result to open the respective line then the file is opened in a new Editor, despite the fact that the same file is already opened in another editor wind...

davhak by Associate II
  • 1504 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.