2022-04-28 6:37 PM
I'm trying to copy a project in cube IDE, version 1.9.0 windows
Very new to using stm32cubeIDE and Eclipse. So I'm hoping I've missed something fundamental, tried a couple of things but no success.
I'm wanting to copy an example that st provide (BLE_p2pServer), but I dont' think that should change the process.
Method 1 - using stm32cubeIDE
1) in IDE I right click on project and copy.
2) I then paste the project (in dialog I rename the project name and use default location).
3) I get error dialog "internal error: null request:"
4) project is only partially copied, the includes look done. But the application folder structure is there but no content.
5) no other folders are copied over :(
6) on my source project if I go to application/user/Core I cannot copy and paste a file from the source project to the new project. I can copy but paste option is not available.
that didn't work.
Method 2 - Export From stm32cubeIDE
1) I select the source project and right click, select export...
2) in export dialog I select General/FileSystem
3) I export to desktop
4) right click in the project explorer and import
5) select import from "projects from folder or Archive", then select the desktop folder that I just exported.
6) Wont' let me import because the project has the same name
7) I rename the folder and now can import, but once i import the project explorer doesn't show anything :(
8) restarted stm32cubeIDE, in project explorer (in ide) I right click and refresh, still nothing
9) try importing this time didn't go with the default and checked the option "add project to working sets", no joy
Method 3 - Manual Method
1) in windows explorer, I copy the source project, rename the folder and rename the .ioc file
2) in IDE I got file/Import project from file system or archive. Select the folder that I just created
3) I have two options the newFolder and the newFolder\STM32CubeIDE. Selected "newFolder\STM32CubeIDE" but nothing happened, so selected newFolder
4) that worked, but the newFolder/project has a different icon for the project and I cannot build it.
Method 4 - Import BLE_p2pServer stm32 example with a different name
1) couldn't find an option to do this :(
I cannot see any other options. Can someone point me in the right direction?
Keen to learn what I need to to solve this. And it might just be my uneducated IDE knowledge.
2022-04-28 9:13 PM
This is a very common question, and unfortunately the answer is that it's not that straightforward, but there are several methods that work.
Insight by ST here:
https://community.st.com/s/question/0D53W00001L1On0SAF/how-can-i-duplicate-a-project-in-stm32cubeide
Oh so many duplicates with answers within:
https://community.st.com/s/question/0D50X0000BqBCOfSQO/issue-when-clone-the-project-in-stm32cubeide
2022-04-28 10:44 PM
Thanks for that TDK, much appreciated.
some of those I had missed and reading them the solution that worked for me was:
https://community.st.com/s/question/0D50X0000BqBCOfSQO/issue-when-clone-the-project-in-stm32cubeide
And the post was by Pavel A, on the February 18, 2020 at 5:05 PM.
I also changed the .cproject file and replaced the old project name to the new one but not sure that this mattered. And seemed to build fine without it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.