STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Separation of STACK and HEAP

Hello,I have a general question regarding the linker script generated by STM32CubeIDE.Most of time the STACK and HEAP is placed together into the "same" internal SRAM (see section .user_heap_stack example for demonstration purpose). Note: Yes, there ...

Floki.1 by Associate II
  • 4639 Views
  • 2 replies
  • 0 kudos

Ethernet communication not working in ST32Cube IDE 1.9.0

Hi,I have a custom board with STM32f427VG and KSZ8041NL PHY. My ethernet communication is working well in STMCube IDE 1.8.0. But when I try to configure ethernet in ver:1.9.0 I don't see a input box for PHY address. It says it some ethernet settings ...

SSala.3 by Associate III
  • 1454 Views
  • 1 replies
  • 0 kudos

Resolved! Login to st.com website fails

I want to download STM32CubeIDE debian version to my laptop. When I click Get Software-->Accept-->Login/Register I get the error " SORRY, PAGE NOT FOUND " . You can see the details at the picture I attached

0693W00000NrUleQAF.png

Post-generation hook in STM32CubeIDE

In our workflow around the code generation and building firmware using STM32CubeIDE, we have certain manual steps after code generation.Is there a place to hook in a script to be run after code generation completes? Similar to the "Build Steps" which...

JKut by Associate II
  • 3128 Views
  • 6 replies
  • 0 kudos

Issue with HAL_Init, my board, or my code?

Hello! I'm using an STM32L4R5ZI board and was running some low power code to put the board in Standby and the board was getting stuck in the clock init section. I would restart the board, it would run HAL_Init (where I assume it would reset the sta...

JayDev by Senior II
  • 3479 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.