2022-06-09 9:39 PM
Hi,
I have a custom board with STM32f427VG and KSZ8041NL PHY. My ethernet communication is working well in STMCube IDE 1.8.0. But when I try to configure ethernet in ver:1.9.0 I don't see a input box for PHY address. It says it some ethernet settings has been moved to LWIP setting page.
How do I set my PHY address which is 1 in STMCube IDE 1.9.0? Is there any more setting to be done compared to 1.8.0 for ethernet communication.
Did anyone face this issue?
Thanks.
2022-06-09 10:52 PM
ST32Cube IDE 1.9.0 has some unfamiliar bug, which I faced with ADC.
my suggestion keep working with 1.8.0.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.