2022-05-19 1:16 AM
Hi everyone,
I want to organise a little bit more our stm32cube projects. I want to remove Src and Inc folders and create some subfolders. Is it doable without having to use your own Makefile to compile the project ?
Thanks in advance for your answer, and sorry if that question has already been answered.
Best Regards,
Thomas
Solved! Go to Solution.
2022-05-19 1:42 AM
It can be done, but you loose the possibility to re-generate the source code pieces generated from the .ioc file. Even if you don't want to re-generate now, you might want to re-generate later to profit from incoming updates.
You are also risking to clutter up the project structure if you accidently re-generate the code.
If you still want to do it, you have to adjust the Paths and Symbols properties of your project to reflect that new folder structure.
[Edit:] It is safe to add new folders and files and leave the generated stuff as is.
hth
KnarfB
2022-05-19 1:42 AM
It can be done, but you loose the possibility to re-generate the source code pieces generated from the .ioc file. Even if you don't want to re-generate now, you might want to re-generate later to profit from incoming updates.
You are also risking to clutter up the project structure if you accidently re-generate the code.
If you still want to do it, you have to adjust the Paths and Symbols properties of your project to reflect that new folder structure.
[Edit:] It is safe to add new folders and files and leave the generated stuff as is.
hth
KnarfB
2022-05-19 6:08 AM
Hi KnarfB,
Thanks for the answer, it's as i thought so that it would not be that simple because of the code generation.
have a nice day,
Best Regards,
Thomas
2022-06-08 4:30 AM
It is only for "STM32Cube" project that you have a fixed project structure.
For Empty and CDT projects you are free to manage the structure of folders and files as you wish.
But no MX auto-generated code in these two project types. ...Just to complete the answer.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.