STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32CubeIDE 1.10.1 released

Fixed issue131250 source files got deleted after project migrationRelated threadsSTM32CubeIDE 1.10.0 Migration IssueHow to avoid project migration issue in STM32CubeMX v6.6.0 and STM32CubeIDE v 1.10.0

STM32CubeIDE shows login dialogs on startup.

Hello, I have just installed v1.9.0 on a new laptop and whenever I start the program I get login dialogs for multiple sites, (for ST, ST SW, Eclipse, etc.) and when I use my normal ST.com login credentials it rejects them. Also when I attempt a soft...

BMohl.1 by Associate II
  • 5674 Views
  • 10 replies
  • 0 kudos

Resolved! Error updating to STM32CubeIde 1.10.0

When I attempts to update STM32CubeIde 1.9.0 to 1.10.0 I get the following errorsAn error occurred while collecting items to be installedsession context was:(profile=STM32CubeIDE, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=,...

0693W00000QKCwpQAH.jpg
RHerm.3 by Associate III
  • 7507 Views
  • 7 replies
  • 0 kudos

Resolved! Including path to linked files doesn't work as expected

I've created an STM32 Project, selected the NUCLEO-G431RB board and generated the code. I've added a source folder to the project (mu_platform) and LINKED some .c and .h files into that folder. I selected mu_platform folder and right-clicked "Add/r...

0693W00000QKVG9QAP.png 0693W00000QKVFzQAP.png

Resolved! Issue with version 1.9.0?

I updated from version 1.8.0 (compilation was ok) to version 1.9.0 where I get 2017 errors :-o.Apparently and issue with ld.exe..tools\arm-none-eabi\bin\ld.exe: SV-F777.elf section `.bss' will not fit in region `SRAM' Processor STM32F777VITxDo you ha...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.