STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Problem with installing the IDE STM32

Good day, gentlemens!I request assistance with installing the STM32 development environment. I have Windows 7 operating system installed, firewall is disabled, no antivirus is present, I'm not using a proxy, and I have a stable wired internet connect...

_legacyfs_online_stmicro_images_0693W00000dK3CuQAK.png _legacyfs_online_stmicro_images_0693W00000dK3DEQA0.png _legacyfs_online_stmicro_images_0693W00000dK3D4QAK.png
SKosi.1 by Associate II
  • 3660 Views
  • 7 replies
  • 0 kudos

LWIP SNTP, what does it actually do?

I am looking in to implimenting a SNTP client on an embedded board, I am using the STM32CubeIDE so its a checkbox to enable SNTP, but I can find no documentation or examples on what you do from there.I can see functions to enable/disable SNTP, but no...

richardh by Associate II
  • 12959 Views
  • 14 replies
  • 0 kudos

STM32CubeIDE crashes when trying to create a new project

Hi,every time I try to create a new project by clicking on "Create a new STM32 project" or "Create a new STM32project from an existing STM32CubeMX configuration file" STM32CubeIDE crashes abruptly. After a few tries I caught the error message with a ...

FKais.2 by Associate
  • 3256 Views
  • 1 replies
  • 0 kudos

Resolved! How to use a Union to access and change the bits?

My header file:typedef union {  struct {    uint8_t u_bit1:1;    uint8_t u_bit2:1;    uint8_t u_bit3:1;    uint8_t u_bit4:1;    uint8_t u_bit5:1;    uint8_t u_bit6:1;    uint8_t u_bit7:1;    uint8_t u_bit8:1;  } bits;} u_serialSequenceBits;My .c file...

LVasc.1 by Associate II
  • 5663 Views
  • 4 replies
  • 0 kudos

After restart device UART_3 printing some rubbish ţ˙ţţţţţţţţüţüüüüüüüüüüüüüüüüüü

Dear,Microcontroler STM32H742 (stm32CubeIDE)When i plug out and plug in device, this printing on UART_3:ţ˙ţţţţţţţţüţüüüüüüüüüüüüüüüüüüor:ţNVT: FF FE FEţţ{FF}i this problem was not watched on same device with stm32F205(Rowley crossworks).I clear all b...

KWiśn.2 by Associate II
  • 7436 Views
  • 18 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.