2023-06-05 5:54 AM
My header file:
typedef union {
struct {
uint8_t u_bit1:1;
uint8_t u_bit2:1;
uint8_t u_bit3:1;
uint8_t u_bit4:1;
uint8_t u_bit5:1;
uint8_t u_bit6:1;
uint8_t u_bit7:1;
uint8_t u_bit8:1;
} bits;
} u_serialSequenceBits;
My .c file:
u_serialSequenceBits myUnion;
myUnion.bits.u_bit2 = 1;
myUnion.bits.u_bit5 = 0;
The Errors:
Description Resource Path Location Type
expected '=', ',', ';', 'asm' or '__attribute__' before '.' token ihm.c /base_UPS_G070v2/Core/Src line 29 C/C++ Problem
Because this commands:
myUnion.bits.u_bit2 = 1;
and
myUnion.bits.u_bit5 = 0;
Solved! Go to Solution.
2023-06-06 1:39 AM
GCC is "Gnu C Compiler", the compiler used by STM32CubeIDE
In C instructions must be inside a function:
void function (void)
{
myUnion.bits.u_bit2 = 1;
myUnion.bits.u_bit5 = 0;
}If you want to initialize the struct at the declaration:
u_serialSequenceBits myUnion =
{
.bits.u_bit2 = 1,
.bits.u_bit5 = 0,
};Pretty much everything related to bit-fields in the C standard is poorly defined. Typically, you will not find anything explicitly addressing the behavior of bit fields, but their behavior is rather specified implicitly, "between the lines". This is why you should avoid using bit fields.
2023-06-05 10:13 AM
I don't get error when I compile your code with GCC
Did you put
myUnion.bits.u_bit2 = 1;
myUnion.bits.u_bit5 = 0;inside a function ?
Show your code around line 29
2023-06-05 3:55 PM
No. It's just inside the source file ".c".
Sorry, i'm a beginner. What's GCC? I'm usign the STM32CubeIDE software.
2023-06-06 1:39 AM
GCC is "Gnu C Compiler", the compiler used by STM32CubeIDE
In C instructions must be inside a function:
void function (void)
{
myUnion.bits.u_bit2 = 1;
myUnion.bits.u_bit5 = 0;
}If you want to initialize the struct at the declaration:
u_serialSequenceBits myUnion =
{
.bits.u_bit2 = 1,
.bits.u_bit5 = 0,
};Pretty much everything related to bit-fields in the C standard is poorly defined. Typically, you will not find anything explicitly addressing the behavior of bit fields, but their behavior is rather specified implicitly, "between the lines". This is why you should avoid using bit fields.
2023-06-06 6:18 AM
It worked, Thanks!
The use of union on my project it's because i want to send a serial data to a 74hc595 and give the manager to change the bits in others .c files.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.