cancel
Showing results for 
Search instead for 
Did you mean: 

PH3-BOOT0

mkm
Associate

Hi,

I am using STM32U585RIT6 MCU & I planned to flash the firmware through SWD and onboard debugger module (STLINK-V3MODS) through VCP.

I am having confusion in configuring the PH3-BOOT0 pin.

Should I connect it to 5V or GND.

Or shall I make it No connect.

@RomainR.  Can you pls help me on this?

Thanks in advance for any suggestions or help

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Diane POMABIA
ST Employee

Hi @mkm 

If you need to boot on the internal flash memory, this pin is set to level LOW (GND) by a pull‑down resistor.

It is possible to put this GPIO to level HIGH to boot on the system flash memory (bootloader), by connecting  this pin to VDD.

Regards

Diane

View solution in original post

1 REPLY 1
Diane POMABIA
ST Employee

Hi @mkm 

If you need to boot on the internal flash memory, this pin is set to level LOW (GND) by a pull‑down resistor.

It is possible to put this GPIO to level HIGH to boot on the system flash memory (bootloader), by connecting  this pin to VDD.

Regards

Diane

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.