STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Error in the Stm32CudeIde program

When generating code, the Code Ide generates the following code:/** Name: cmsis_os2.c* Purpose: CMSIS RTOS2 wrapper for FreeRTOS*/...osStatus_t osThreadTerminate (osThreadId_t thread_id) {TaskHandle_t hTask = (TaskHandle_t)thread_id;osStatus_t stat;#...

juvf1 by Associate
  • 2329 Views
  • 2 replies
  • 2 kudos

VCPKG fails with STM32 VS Code Extension

Hi,Trying to get he new STM32 Extension working for VS Code and it is failing with> Using vcpkg executable at "/home/iwiseman/.vscode/extensions/ms-vscode.vscode-embedded-tools-0.7.0-linux-x64/assets/platform/linux-x64/vcpkg-glibc.app". > Using VCPK...

bibble235 by Associate III
  • 6039 Views
  • 3 replies
  • 2 kudos

Resolved! Pointer to cyclic buffer at stm32H7A3

I am running ADC DMA in cyclic modeat STM32G474CET6  Im useingBuffer_Addr_At_Trigger[ ADC_Loop_Counter] = hdma_adc1.Instance->CNDTR;to read the pointer of the cyclic bufferIn the STM32H7 familyAn syntax error for CNDTRI can't find the appropriate reg...

hroze.1 by Associate II
  • 2090 Views
  • 3 replies
  • 1 kudos

NUCLEO-F756ZG ethernet CubeIDE configuration

Hello all!help needed! :)For last week I try to make UDP server on NUCLEO-F756ZG.I am stuck in the beginning...I can't configure my board to ping it.From reading old threads I understand that there was an issue with automatic ethernet configuration o...

AKhar.5 by Associate II
  • 3813 Views
  • 5 replies
  • 0 kudos

XCore407i

Estoy tratando de iniciar con la board XCore407I, descargue el ide ST32CubeIDE pero quiero generar un nuevo proyecto en Board Selector no esta XCore407I.Que puedo hacer???

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.