STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

DCACHE on STM32U599

Hi!I'm configuring the STM32U599VJT with CubeMX enabling DCACHE1 and 2, as well as ICACHE. Code is generated without error, but functions like SCB_CleanDCache_by_Addr() are not enabled as the definitions in stm32u599xx.h do not include __ICACHE_PRESE...

paolog by Senior
  • 3600 Views
  • 4 replies
  • 1 kudos

lwIP deadlock with a twist

Setup:MCU: STM32F429PHY: DP83848 (MII)Advertised Mode: 10BASE-T, Half/Full-Duplex 100BASE-TX, Hal/Full-DuplexOS: CMSIS-RTOSv2CubeMX: Yes Just wanted to start of with mentioning that i've read and tried the fixes  provided by @Piranha. I've tried the ...

XD by Associate III
  • 3701 Views
  • 4 replies
  • 0 kudos

HardFault_Handler

Hello,until recently, I used the STM32F411CEU6 microcontroller; lately, I switched to the STM32G0B1.I've ported the old C++ code from the STM32F411CEU6 to the STM32G0B1.Everything works correctly; the only issue is that now, 'HardFault_Handler()' occ...

Resolved! In STM32CubeIDE How can I fix "arm-none-eabi-gcc: fatal error: cannot execute 'cc1': CreateProcess: No such file or directory"

When I create the default project for the NUCLEO-F429ZI board and build without any edits I get the following error repeatedly and would like to get rid of it. I can build the same on a different laptop. How can I solve this problem. "arm-none-eab...

jdsotack by Associate II
  • 11039 Views
  • 3 replies
  • 2 kudos

ADC

how to use multiple adc in stm32f746zg nucleo board

STM32CubeIDE 1.14 and Darkest Dark Theme with DevStyle

I uninstall IDE v1.13 and install the new v1.4 from the ST website.Installation without problems, but already at the first launch I see that instead of the Information Center page it says "the page cannot be displayed".When I try to download Darkest ...

KHans.4 by Associate
  • 3289 Views
  • 1 replies
  • 0 kudos

Resolved! ThreadX priority

Hi guys. Help solve this problem.I am working with STM32H745 and ThreadX. In my project, an external event generates an interrupt on EXTI10.The tx_event_flags_set() function is executed from the HAL_GPIO_EXTI_Callback() interrupt handler to start a p...

Resolved! STM32g0xx change boot address with option bytes

Hi, I used this code to change the boot address in the STM32U575 project:FLASH_OBProgramInitTypeDef OB_Data;/* Unlock Flash Control register and Option Bytes */HAL_FLASH_Unlock();HAL_FLASH_OB_Unlock();OB_Data.OptionType = OPTIONBYTE_USER | OPTIONBYTE...

MishKa59 by Associate III
  • 2116 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.