STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

unable to debug stm32f508-dk

sir i am trying to read and write 10 bytes of data into flash memory, before that iam going to debug the code ,am getting this error "No source available for "_binary_______ExtMem_Boot_Binary_Bootloader_bin_start() at 0x8001ece" "

kishor by Associate II
  • 2152 Views
  • 3 replies
  • 0 kudos

Multiple errors reported.

Hi, currently I have an issue during debug. I'm writing a bare metal code to blink a LED, when I compile the code there aren't any error occur. But when check the Expression I got this errors, I have search everywhere but I can't find the solution ye...

trietmt9_0-1702304937876.png
trietmt9 by Associate II
  • 3840 Views
  • 5 replies
  • 1 kudos

Resolved! Indexer crash

I'm failing to get the indexer working correctly.So far I've tried several solutions regarding paths definition and Eclipse memory sizes allocation. All of them leading to the same error for all the files in my project. See an extract of the .log fil...

O'li by Associate II
  • 1930 Views
  • 1 replies
  • 0 kudos

ADC value is not being read

Hi all, I am new to stm32cube ide and this is my first project. I am currently working on stm32f103c8. I am taking the input from ADC1 pin PA0 which is connected to a potentiometer. I am controlling LEDs through a potentiometer and a button. The prob...

Resolved! Compiler can't find files, even though paths are included

I am trying to implement TinyUSB in an STM32CubeIDE project. My current problem, where I am quite stuck, is that the compiler can't find functions located in the TinyUSB folder tree. Example: ../Core/Src/main.c:176: undefined reference to `tusb_init'...

EThom3_0-1702132473439.png EThom3_1-1702133262402.png
EThom.3 by Senior III
  • 8024 Views
  • 2 replies
  • 4 kudos

ETH HTTP

Hello, I would like some advice. I have created an http web page which can only be accessed if on the same network. But what if I want to access a web page outside the network? What do I have to do? From my research, a forward port is used to allow e...

non by Associate III
  • 2855 Views
  • 3 replies
  • 0 kudos

How to use multiple Timers?

how to use multiple timers in stm32f746zg,i am using timer1 and timer4 as PWM generate and i am using timer2 for sdcard but it is not working that controller get struck and again i want to re-upload the code if the press the reset button also it is n...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.