STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Can't find Nucleo-MB1549 in board selection

I'm used to using the stm32cube-ide. I found a Nucleo-MB1549 in my attic and wanted to play around with it but i can't seem to find it in the board selector section.  Any ideas what i should do next? This is a genuine nucleo board and i am able to fi...

BadEngineer_0-1721771231250.png

STM32CubeIDE v1.12.0 disassembly addresses change

Bug ReportWhen I look at the disassembly of my code, the addresses seem normal. As soon as I scroll through the disassembly, all the addresses change from even to uneven. Further scrolling does not change the addresses back. We look at the disassembl...

JWend.1 by Associate II
  • 2948 Views
  • 2 replies
  • 2 kudos

Resolved! Internal browser greyed out

Hy all,I'm experiencing a problem with the internal browser of the CubeIDE.Starting from the beginning:I freshly installed Opensuse 15.6, to override a problem generated by an upgrade went wrong.After the OS was fine, I installed all the applications...

SS_CubeIDE.png SS_CubeIDE_2.png
rdipra65 by Associate
  • 1624 Views
  • 1 replies
  • 0 kudos

Can't set a breakpoint in debug

I'm working with an STM32U575 Nucleo and also a custom board with the same processor.In STM32CubeIDE, neither project will let me set a breakpoint. What am I missing?I've attached a screenshot showing a "broken" breakpoint.

DeInitialization of the QSPI peripheral

I intend to use the following API to deinitialize the OCTOSPI peripheral which I am using in the Quad SPI mode on the STM32H563 board:  HAL_StatusTypeDef HAL_XSPI_DeInit(XSPI_HandleTypeDef *hxspi) { HAL_StatusTypeDef status = HAL_OK; /* Check th...

AShetty by Associate II
  • 1680 Views
  • 2 replies
  • 0 kudos

STM32CubeIDE - Auto-complete (Ctrl+Space) is not working

Hello, I installed STM32CubeIDE and imported (a copy) of a TS project.Quickly, I hit an issue: auto-complete proposals (Ctrl+Space) gave no proposals in STM32CubeIDE. The pop-up window only shows 'No Default Proposals'  UPDATE: I fixed it, the prefer...

Jack3 by Senior III
  • 22605 Views
  • 14 replies
  • 19 kudos

How to setup QSPI file sytem on Norflash

HI, All     I am testing file system on U575 Eval board. The file system is working when I setup the connectivity  to Norflash as Oct2SPI. However, when I changed the connectivity to QSPI, it failed at the initialisation of format as the following:my...

Victorheca01_0-1721665364507.png Victorheca01_1-1721665412254.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.