STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Can't get Printf to work on CubeIDE

Currently using a STM32L4R9I-DISCO and I've been struggling to get the SWV ITNM Data Console to work so I can do some debugging. I'm quite new to this, but I've followed every tutorial online to enable UART and how to set it all up, to no avail. I've...

Hafez1 by Associate III
  • 10772 Views
  • 13 replies
  • 5 kudos

STM32H750 Reboot

Hello, I am working on a STM32H750. Since the flash is limited, I implement a bootloader and an application. The application is programmed into an external flash. When I am developing the application with STM32CUBEIDE, I have to reboot the board manu...

hbZhao by Associate III
  • 1349 Views
  • 1 replies
  • 0 kudos

Resolved! STM32H750 Copy to ITCM without GCC "Copy to NULL" warning

I see lots of posts with folk struggling to get code into ITCM, but not the (sorta) problem I have after getting things working.  It is just a compiler warning, but I'd like to find an elegant way of handling it.The issue is I am using memcpy to copy...

Will5 by Associate III
  • 2847 Views
  • 5 replies
  • 1 kudos

Can we use CAN FD for sending 3000byte of data

Hello,Our Application need to send 3000 bytes of data over CAN busCAN FD allows us to send 64 bytes of data in one frameIs it feasible to use CAN FD for our application?Is there any other way, which we can use in CAN?Also can we use the Multiframe co...

Resolved! How To Play Digitally Generated Sine Wave

I just finish a TouchGFX code to generate an adjustable sine wave. I am planning to make 3 of them to mix them and play chords but there is a problem: how can i play a function that generated in STM32 on the speakers of that STM32?I would be so glad ...

Nhyrane by Associate II
  • 4307 Views
  • 6 replies
  • 7 kudos

USE_BSP_COM_FEATURE > 0 on B-U585i-IOT02A

Hello forum,I'm trying to use the BSP driver while implementing a USB Host functionality. after the initiation of everything the USB needs, the BSP started to raise a lot of errors of undeclared/undefined stuff, after checking I saw that the error wa...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.