STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

USBX code not compiling after IDE generation

Using STM32 Cube IDE v1.15.1 with package stm32u5-1.5.0 or IDE 1.16.0 with package 1.6.0 (Linux and Windows versions) :Create new STM32 project from example Ux_Device_CDC_ACM for board Nucleo-U5A6ZJ-QCompile project : okSlight modification in IOC fil...

DBGMCU_CR_DBG_STOP setting ignored

Setting DBGMCU->CR.DBGMCU_CR_DBG_STOP should allow debugging in STOP mode; eg, from ST examples: /* Allow debugging in Stop Mode */ DBGMCU->CR |= DBGMCU_CR_DBG_STOP; /* Enter Stop Mode */ HAL_PWR_EnterSTOPMode( PWR_LOWPOWERREGULATOR_ON, PWR_S...

AndrewNeil_0-1701710496575.png

Cubeide deletes files if disk is full

So weird behaviour: my disk was running full, while i was modifying a file. When trying to save instead of aborting it just emptied the whole file, what a *** weird behaviour, other editors would just do nothing. 

TwixMeow by Associate
  • 1133 Views
  • 1 replies
  • 0 kudos

Extern variable error

Hello,I'd like to use some extern variables in my code, but I always get the error "undefined reference to ..." and I can't find what I am doing wrong.In the timer.h file I declare the variable as: extern volatile uint8_t start_adc_flag;I included th...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.