STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! No capture IT triggered

Hi,Something seems to be wrong with STMCubeIDE Version: 1.16.0 Build: 21983_20240628_1741 (UTC) with an STM32G070RBT6. After generation of the code, the Timer code is like this:/*** @brief TIM3 Initialization Function* @param None* @retval None*/stat...

Gaetan by Associate
  • 1758 Views
  • 2 replies
  • 1 kudos

Code Coverage Gcov Lcov

Hello,is anyone able to generate a lcov coverage report in Stm32cubeIde or to visualize the the coverage result inside the editor?I have the *.gcno and *.gcda file (by semihosting). Regards Peter

PPete by Associate III
  • 2293 Views
  • 1 replies
  • 0 kudos

Resolved! Bad code generation with ADC LL API and STM32CubeIDE

I recently changed the configuration of working product from HAL API to LL API to improve performances.Unfortunately, the LL initialisation code generated by the STM32CubeIDE for the ADC was incomplete, and forgets to set the PCSEL register when need...

cberg.1 by Associate II
  • 2426 Views
  • 3 replies
  • 0 kudos

Resolved! STM32F1 with EasyCAT

Hello~I am testing my stm32f103rb board with ethercat board(as shown). The trouble i am having is that there is no easycat library to use. I did some research and only found the .cpp easycat library. I'm using stm32ide and written in C language. This...

arduino-uno-rev-3-easycat.jpg
ANHTUAN by Associate
  • 2372 Views
  • 2 replies
  • 1 kudos

STM32CubeIDE locks up on Java

HiI have STM32CubeIDE 1.16.0 installed on Ubuntu 22.04.4 on a DELL with Intel i7. Whenever I close the IDE with the MX interface open, it cannot start again, and it complains about Java. It is probably an Eclipse error, but it is a bit of a pain. I k...

ErikLea by Associate
  • 846 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.