STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Compile problems because of linked resources

I update to V1.16 and found, that my project cannot compile anymore.Problem are compile errors, double definitions and so on. I did not change the code, just updated and regenerated everything include the code generation of CubeMX ( from within the i...

SThie.1 by Associate II
  • 1492 Views
  • 1 replies
  • 0 kudos

STMCube32 IDE - license terms not readable

When installing for example the Nx_MQTT example for B-U585IOT02A you need accept a license for CubeFW U5 1.6.0. You are supposed to view it 1st. However, at least with Ubuntu 22.04 and FireFox as default browser (default for Ubuntu 22.04) you can't v...

JanneKiiskila_0-1724071861149.png JanneKiiskila_1-1724071900551.png

STM32Cube ID 1.16.0 - uninstall.sh missing?

I have been asked to remove (uninstall) the STM32Cube IDE and replace it with another version. However, the instructions found how to uinstall STM32Cube IDE suggest there should be an uninstall.sh script in the /opt/st/STM32CubeIDE_<version> -folder....

Resolved! (M24M01E-F) Data storage

Hi,For my project, I am using an M24M01E-F I2C EEPROM. In this application need to store sensors offset values (float data type) in EEPROM. whether it can be able to write/ read float value. Regards,Rishvana M

Rishvana by Associate II
  • 1555 Views
  • 2 replies
  • 1 kudos

Broken server install / Debian 12.5 Bookworm

Hi,Recently, when I tried to install the Debian Linux version of STM32CubeF4 on my Debian Linux (v12.5) Bookworm system, I began by trying to install a package that included Server 2 in its name. The server install hung at 50% installed. Each time I ...

How can I change the build analyzer color preferences?

I use the dark theme of the IDE and can find no preference settings to change the colors for the build analyzer output. The IDE shows the usage info with light gray text on a bright green background which (to my eyes) is almost unreadable. I say almo...

Build Analyzer Color Preferences.PNG
DSudo.2 by Associate III
  • 1480 Views
  • 1 replies
  • 0 kudos

Convenience of CubeIDE

It is done incorrectly that after pressing the "Debug" button while the project is being compiled and loaded into the MCU - it remains possible to press the "Debug" button again, which is incorrect (this will corrupt the normal course of the process)...

OlegAjax_0-1723713520475.png
OlegAjax by Associate II
  • 1161 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.