STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

ITM Debug with SWV H755

I am unable to get ITM debug working via either CubeIDE or Cube programmer.  I have checked the sysclock matches the sysclock configured for the system.I have tried various limits and auto for the SWV clock.I have enabled SWV in the debugger config.I...

tstokes_0-1728309818225.png tstokes_1-1728309947212.png
tstokes by Associate III
  • 1810 Views
  • 2 replies
  • 0 kudos

Resolved! Program size calculation using STM32CubeIDE

 Hi, When compiling program using Keil IDE, understand that the program size that flash to MCU can be calculate by:Program size = Code + RO + RWHowever, when compiling using STM32CubeIDE, how to know the program size going to flash into the MCU flash...

chai2145_1-1728379506281.png

Error: Code generation could not be done because the necessary firmware package is missing. Not able to complete STM32Cube project creation.

I hope this is the right thread for my question. I recently decided to switch to STM32CubeIDE from the online compiler as there is debugging and is offline capable.I downloaded STM32CubeIDE and went to create a new STM32 Project. I selected my dev bo...

0693W000006F5mEQAS.png 0693W000006F5n2QAC.png 0693W000006F5nqQAC.png
CWill.3 by Associate II
  • 16393 Views
  • 18 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.