STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

CubeIDE Memory view - why different fonts?

Why am I getting 2 different fonts in these Memory views?If I now create a new view, it uses a different font: It seems that it only happens in a newly-created view; if I switch from that last one to one of the earlier views, then switch back again, ...

AndrewNeil_0-1728052642767.png AndrewNeil_1-1728052675908.png AndrewNeil_2-1728052764836.png AndrewNeil_3-1728052915084.png

Resolved! STM32IDE cannot sometimes find an included linker file

I have a complex project that has multiple sub-projects inside. One of these projects has an additional .ld file called "STM32L431KCUX_SHARED.ld". This file is a linked resource in other sub-projects and normally it works without an issue, every "STM...

MO94 by Associate III
  • 4752 Views
  • 4 replies
  • 1 kudos

Handler Semaphore in STM32

Hello, I'm having an error and need helpIn NormalTask, I am getting an error at line 250. I want to hold the Semaphore and when I press the button, it will release the Semaphore. The error I'm getting is that the task automatically releases the Semap...

noname8888_0-1728265570653.png

Resolved! How to generate *.bin file after building with CubeIDE?

Hello Cube IDE teamI am using STM32F427ZG MCU board with STM32CubeIDEBut I have trouble to generate *.bin file after building with CubeIDE.I think it support *.elf file only for now.If below command can be added into makefile, then *.bin file can be ...

0690X000008B9YlQAK.png
CARHERO by Associate III
  • 40387 Views
  • 8 replies
  • 10 kudos

STM32 Cube IDE Software Breakpoint

Hi, How to put the software breakpoints in the STM32 Cube IDE. I can put only the hardware breakpoints. The hardware breakpoints has a limitation of maximum 5. We can use multiple software breakpoints in the STM8 Chips with ST Visual Development IDE ...

NM by Associate III
  • 3720 Views
  • 6 replies
  • 1 kudos

Resolved! STM32CUBEIDE install error

It doesn't install as the phrase pops up. "can't initialize plugins directory. please try again later​" I've tried everything. Please help me.window10 64bitintel core i7-6700 3.4GHz

0693W000004Ik7yQAC.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.