STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Cannot activate IRTIM peripheral

Hi, I'm developing an application based on STM32U031K8. I need to use the IRTIM peripheral to create an IR transmitter. I set TIM15_CH1 and TIM16_CH1 as "Output Compare No Output" but IRTIM peripheral still cannot be activated. May someone help me?

aerauliqa by Associate II
  • 3394 Views
  • 8 replies
  • 0 kudos

Resolved! STM32 cube IDE Debugger error

I have created a demo project using touch gfx I'm able to flash that project using touch gfx. But when I try to flash that project using Stm32Cube ide it raises an error like "Failed to execute M1 command". Please refer attachments for more details.

sai1 by Associate II
  • 4308 Views
  • 5 replies
  • 3 kudos

About Timer work after Stop mode with RTC

Hello,Once I thougt I measure the duration time after entering Stop mode with RTC to wakeup by EXTI interupt on the STM32L0538-Discovery.But I noticed any timers don't work during Stop mode, is this right?And I think after entering Stop mode, any var...

curiae by Associate III
  • 2941 Views
  • 7 replies
  • 1 kudos

Resolved! Internet connection

Hello,Im unable to connect to internet in IDE and MX. Check below image in IDEBelow seen in MXMy work is getting hampered due to this. Please let me know what to do.

GauravK_0-1727273256884.png GauravK_1-1727273359373.png GauravK_2-1727273375566.png
GauravK by Senior
  • 6257 Views
  • 7 replies
  • 1 kudos

USB Protocol

I am using STM32F423RHT6 in the project. In .ioc file, there are different versions of USB being given. I am getting confused in which is given for what purpose?  Under the connectivity tab, there is USB OTG FS, whereas in Middlewares and Softwares a...

Screenshot 2024-10-08 165743.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.