STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Issue with BSP Configurator

I am trying to create some example code for a Nucleo G474RE board and one of the initialization steps was whether I would like to use the BSP for the Virtual COM port, user LED and user button. Note that this is what the configuration looks like Buil...

AdamHamilton_0-1731836258352.png

Unable to download STM32CubeIDE

I'm having an issue of downloading CubeIDE, I'am using FireFox to download Cube IDE. Each iteration it stops at around 545MB of downloading. I haven't kept any download limit to any of my devices. It happens for all files in the download list. Please...

Yadavrao by Associate
  • 1250 Views
  • 2 replies
  • 0 kudos

Export Application Example

HiI started working with the openbootloader and the application example located here:\STM32Cube\Repository\STM32Cube_FW_G4_V1.6.1\Projects\STM32G474E-EVAL\Applications\OpenBootloaderThe example works fine, and I managed to get everything to run. I ha...

DeIng11 by Associate
  • 1014 Views
  • 1 replies
  • 0 kudos

Resolved! network connection required message box appeared

hi,      I am  unable to connect to internet in STm32 Cube IDE and i am not running any proxy server,and I tried changing network connections settings like manual, native and  Direct, but same issue faced.what can i do? how to solve my problem 

Screenshot 2024-11-29 091733.png

cubeide debug without downloading

ST Technical Support:    I have encountered a strange question and have not yet found the answer. When using Cubeide, I only wanted to debug the hardware but didn't want to write flash, which was supposed to be a simple task, but I failed. Using the ...

Can't see memory uage at Build Analyzer

Hello! I have a STM32CubeIDE project that I run on a STM32WB5MMG module.I program it in debug mode and set a breakpoint in the code.When I open Build Analyzer it's empty. When I see other people open it, they get information about RAM usage. What hav...

DLid1_0-1713623582109.png
DLid.1 by Associate II
  • 9441 Views
  • 6 replies
  • 19 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.