STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32CubeIDE - can't connect to download package

Title edited to be more descriptive; post moved to the CubeIDE section.Just installed stm32cube ide and created a new project. It said I needed to connect my st account to download a package or something. When I try and connect my account I get this ...

jasonbm123_0-1734459967953.png

Resolved! Can't build existing projects after upgrading Cube IDE

I've just upgraded from Cube IDE 1.15 to 1.17.0 under Ubuntu 22.04 using the 'check for updates' feature.When I try to rebuild (right click in project explorer and click 'build project') any of my existing projects I just get a message such as below....

TJack.2 by Associate III
  • 3128 Views
  • 4 replies
  • 2 kudos

SWV Timeline error -500000000

Hi,when I am plotting data with SWV timeline, the timeline randomly plots -500000000 or lower values, while plotted variable does not drop that low. Don't you know, where could be the problem? I did the easiest program, but the SWV still has this err...

Resolved! Linux Installation Error - STM32 Cube IDE

I have a VM running with Ubuntu 22.04 -- a brand new, clean installation.In case it matters...The host machine is a Mac M3I actually had this running some time ago, but have since deleted the VMI am working with an offshore team doing some dev work f...

sparrow by Associate II
  • 4759 Views
  • 5 replies
  • 1 kudos

CubeIDE Debug Application with BootLoader

I am porting over an application from SystemWorkbench to CubeIDE. This application has a bootloader and application. The application is loaded at 0x08008000. With SystemWorkbench I added a linker flag of -nmagic, but in CubeIDE that throws an error. ...

Stephen28 by Associate III
  • 6168 Views
  • 6 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.