STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

RTOS Aware Debug

IDE VERSION: v1.14.1+Target: STM32H750Debugger: ST-LinkSo, 98.9% of the time I try to enable RTOS aware while debugging using the ST-Link I receive this message:After that, I'm no longer able to debug code. This is normally "worked around" by closing...

rmartins_0-1741035795145.png
rmartins by Associate II
  • 1167 Views
  • 2 replies
  • 0 kudos

Resolved! Issue with Code Generation in STM32CubeIDE for STM32H747

Hi everyone,I'm working on a project with STM32CubeIDE and an STM32H747 microcontroller. I've configured the clock sources in the .ioc file as follows:High Speed Clock (HSE): BYPASS Clock SourceLow Speed Clock (LSE): Crystal/Ceramic Resonator  When I...

SSerg4_0-1741119975325.png
SSerg.4 by Associate III
  • 1432 Views
  • 2 replies
  • 1 kudos

Resolved! CudeIDE , does'nt generate any Code File

Hallo Everyone,i am kindly new on STM and i am starting with some Basics programming stuff using a Ubuntu PC and  the NUCLEO-F401RE. However after installing the Ubuntu Version with the "STM32CubeIDE Debian Linux Installer",  i started a new Projekt ...

Screenshot from 2025-03-04 12-51-56.png Screenshot from 2025-03-04 12-38-40.png Screenshot from 2025-03-04 12-38-13.png
kgb by Associate III
  • 1482 Views
  • 2 replies
  • 1 kudos

Resolved! No way to Log into MyST on CubeIDE V 18 ??

Hi,I upgraded CubeIDE to V.18 but when creating a project from an IOC file it could not generate any code because the micros packages are missing. It said to log into MyST but there is no Login option where it previously was (see screenshot below).Ho...

Ricko_0-1741031489011.png
Ricko by Senior III
  • 2151 Views
  • 3 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.