2025-03-03 3:46 PM
When attempting to configure TIM1 channel 4 to "PWM Generation CH4 CH4N" to operate on PE15 for the eval board, the code in tim.c will include the following:
However, the definition used, GPIO_AF3_TIM1, is a HAL library definition instead of "LL_GPIO_AF_3", which is the correct LL definition (in both cases, the value is 0x3h). If both the HAL and LL drivers are used, this may still compile, however if only using LL drivers without the HAL, it will throw a compile time error.
2025-03-03 11:26 PM - edited 2025-03-06 5:44 AM
Hello @jackalope ,
First let me thank you for posting and welcome to the ST Community.
Your request is under investigation, and I will get back to you ASAP.
I suggest also that you provide the MCU reference.
Thanks.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.