STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

TrustZone Secure Debug

I have a project with TrustZone enabled, and am able to debug the non-secure side fine, but breakpoints never hit on the secure side (functions through nsc from non-secure side) other than main before it jumps to the non-secure side. I'm setting it u...

JamesB_0-1740782581863.png JamesB_1-1740782621853.png JamesB_2-1740782696050.png
JamesB by Associate II
  • 1495 Views
  • 2 replies
  • 0 kudos

I need download 1.6.1

Hi Imen,   The link is not working anymore, can you share it again?I would need STM32CubeIDE 1.6.1 as well

jdn by Associate
  • 778 Views
  • 1 replies
  • 0 kudos

Minimum Heap Size has no effect on linker file

When I make a change to the Minimum Heap Size setting in the ioc file (STM32CubeIDE 1.16.1) for G071RBTX, it results in no change to the linker file. However, changing the Minimum Stack Size here does cause a change in the liker file. What does the M...

Carl_G by Senior III
  • 1376 Views
  • 2 replies
  • 1 kudos

Next version of GNU Tools for STM32 release date?

Hello,I've seen that there is a GCC 12.3 version of GNU Tools for STM32 in the repository  here: https://github.com/STMicroelectronics/gnu-tools-for-stm32.When can I expect this to be released in an official STM32CubeIDE/CubeCLT version?Does this rep...

Nico1 by Associate II
  • 6570 Views
  • 9 replies
  • 8 kudos

Resolved! XPSR register bitfields?

Is there a way to split the XPSR register view up so you can see each status bit by its name rather than the 32-bit value?The SFRs have this feature, why do the general registers not have it enabled by default?

Synchronizing PWM Signal through an external Signal

I'm using NucleoG071RB for this experiment. I have an (periodic) external signal that should reset the Timer counter to zero, so that the PWM is synchronized to the external signal. I used the external signal to generate an interrupt (EXTI), and rese...

MIXA1 by Associate
  • 1091 Views
  • 1 replies
  • 0 kudos

STM32CubeIDE IOC Interface Unusable with STM32N6

I started a project based on the STM32N657X0H3Q.  The .IOC file gets generated.  I was trying to search for various pins.  I typed in "PA0" . . . all OK . . . continued with other PAX pins.  After a while, the user interface became more and more slug...

MHenz by Associate III
  • 1039 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.