STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! STM32CubeIDE Voltage Sensor with STM32F103C8T6

The is voltage sensing in live expression I'm using STM32F103C8T6 board popularly known as blue pill im using a voltage divider the supply is given from the power supply and the ADC pin i use is B1 from the power supply when i give less than 2V the o...

Resolved! How to program Blue Pill (STM32F103C8T6) using C++ on STM32Cube IDE to blink its LED as the first embedded project

Hi all,This is my first embedded programming project and Blue Pill is my first board to work on. Since I've got some experience in C++, I wish to use that language to make a project for blinking the Blue Pill's LED. Amongst various IDEs out there I p...

Adev.1 by Associate III
  • 2781 Views
  • 1 replies
  • 0 kudos

Resolved! Blue pill does not have DAC in Cube

Hi AllToday I wanted to start working with Bluepill DAC that turn out in STM32CubeIDE there is no DAC peripheral and I was shocked. Does anyone know what the h... is that issue? and how to solve it? I don't like to configure it by myself.

IDavo.1 by Associate II
  • 4187 Views
  • 5 replies
  • 0 kudos

Resolved! unable to erase flash stm32h7b0

hi. i want to write a variable into stm32h7b0vbt6 flash memory and all of the hal source and header files are added to project. so i have used FLASH_EraseInitTypeDef to erase flash first.but when i call that, the program not build and shows this erro...

code.png errors.png

Program "-E" not found in PATH-STM32cubeIDE

您好,我遇到了一个非常棘手的问题。(STM32cubeIDE)当我打开朋友给的项目时,我在点击打开项目时遇到了以下问题。你能帮我解决吗? Translation: "Hello, I have encountered a very tricky problem. (STM32cubeIDE) When I opened the project given by my friend, I encountered the following problem when I clicked to ope...

zhangJJ_0-1745497822776.png
zhangJJ by Associate
  • 768 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.