STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Newbie, question about opening cube

Edit by ST Moderator: This post has been translated from Chinese to comply with the ST Community Terms and Conditions (§10.2). Why is it that after turning off the computer after downloading and using it, and turning it on again, the cube won't open ...

Resolved! HAL_ADCEx_Calibration_Start

Just a question: I'm using the following code snippet: void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim) { if (htim == mod_timer){ pwm_timer->Instance->CCR4 = sinetab[loop_cnt++]*global_adc1/4096.; //setzt neuen PWM-Wert aus Tabelle ...

ide Version v.1.18.1 external loader issue

hi,stm32h723zgt6 + W125Q128 + v2 stlink was working fine with  V.1.17.0. i had external loader issue with  V.1.18.0 version update and i was reported as well as in the past month .I knew downgrading ide version to  V.1.17.0 is the solution but my PC ...

MMARI.1 by Senior II
  • 805 Views
  • 0 replies
  • 0 kudos

How do I update the CMSIS used by a project?

I've created a project for an STM32G031 device, but the code does not build cleanly with -Wsign-conversion due to some "nasty" stuff in the CMSIS core_cm0plus.h file:../Drivers/CMSIS/Include/core_cm0plus.h: In function '__NVIC_SetVector': ../Drivers/...

CTapp.1 by Senior III
  • 1495 Views
  • 2 replies
  • 0 kudos

Resolved! Measure the speed rotation by using TIM in encoder mode

hello, I ask for the following clarification: I am using a two-channel encoder, A and B, and I want to estimate the rotation speed of the encoder shaft as precisely as possible. I started setting the TIM2 in encoder mode.My encoder generates 1200 pul...

SMusc.1 by Senior
  • 5302 Views
  • 14 replies
  • 1 kudos

Resolved! STMCUBE IDE can we use two debug window at time?

Hello, I am using the NUCLEO-h745ziq board. I am using two board for SPI loopbacking.One board as master and one board as SLAVE. Can we use the two debug window at time. Because I launch the one stmcubeIDE window 1.5.1 and another from stmcubeide 1.6...

MDeva.1 by Associate II
  • 6416 Views
  • 4 replies
  • 5 kudos

Resolved! STM32F103 Nucleo Pushbutton RTC Conflict

Hello,I've discovered the following anomalous behavior when attempting to use the STM32F103 Nucleo board:Pushbutton interrupt code will not execute if the RTC is active with NVIC EXTI13.  I've noticed that the RTC tamper PIN is also assigned to PC13 ...

Resolved! IDE Theme and appearance

How to change this theme, i couldn't find any settings related to this, i have tried all the colors and font settings, it comes default after installing STM cube IDE as fresh start. Somebody please help with this ?i have tried with ecllipse marketpla...

peradheep_0-1745168125804.png
peradheep by Associate II
  • 2525 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.