2025-04-01 5:40 AM - edited 2025-04-01 9:22 AM
Executed from the linux tree root where the kernel was build from
The dts was placed in the arch/arm/boot/dts/st/ folder. {STM32MP_PROJECT} is the filename (and hardcoding the dt filename gives the same result)
Followed the wiki and the kernel HOWTO readme (both have different instructions)
https://wiki.st.com/stm32mpu/wiki/How_to_compile_the_device_tree_with_the_Developer_Package
make V=1 ARCH=arm st/stm32mp157a-dk1.dtb LOADADDR=0xC2000040 O="${OUTPUT_BUILD_DIR}"
OK
make V=1 ARCH=arm st/${STM32MP_PROJECT}.dtb LOADADDR=0xC2000040 O="${OUTPUT_BUILD_DIR}"
FAILS
make ${IMAGE_KERNEL} O="${OUTPUT_BUILD_DIR}" KBUILD_EXTDTS="${EXTDT_DIR}/linux" ${STM32MP_PROJECT}.dtb
FAILS
The error reported is No rule to make ... etc..
Since ECO 6.0 boards are now in subfolders under configs. ST's dt's in the same folder compile fine. The file is there with the correct name. Make/Makefile seems to execute some kind of scripts which i can't follow. Perhaps custom DT's not in the Makefile were never tested/considered ? P.S Why is there a LOADADDR needed for this ?
Solved! Go to Solution.
2025-04-02 12:28 AM - edited 2025-04-02 12:30 AM
Hello @debugging ,
From what I understand, you added manually your device tree into kernel sources "in tree". In this context, you do not have to use the last compilation command you gave as this is for External device tree purpose.
Your error let me think about a missing dtb added in the Makefile of the same folder. Did you well add it below the other STM32 ones ?
stm32mp157f-dk2-a7-examples.dtb \
stm32mp157f-dk2-m4-examples.dtb \
stm32mp157f-ed1.dtb \
stm32mp157f-ev1.dtb \
stm32mp157f-ev1-a7-examples.dtb \
stm32mp157f-ev1-m4-examples.dtb \
YOUR_DT.dtb \
dtb-$(CONFIG_ARCH_U8500) += \
ste-snowball.dtb \
ste-hrefprev60-stuib.dtb \
ste-hrefprev60-tvk.dtb \
ste-hrefv60plus-stuib.dtb \
Kind regards,
Erwan.
2025-04-02 12:28 AM - edited 2025-04-02 12:30 AM
Hello @debugging ,
From what I understand, you added manually your device tree into kernel sources "in tree". In this context, you do not have to use the last compilation command you gave as this is for External device tree purpose.
Your error let me think about a missing dtb added in the Makefile of the same folder. Did you well add it below the other STM32 ones ?
stm32mp157f-dk2-a7-examples.dtb \
stm32mp157f-dk2-m4-examples.dtb \
stm32mp157f-ed1.dtb \
stm32mp157f-ev1.dtb \
stm32mp157f-ev1-a7-examples.dtb \
stm32mp157f-ev1-m4-examples.dtb \
YOUR_DT.dtb \
dtb-$(CONFIG_ARCH_U8500) += \
ste-snowball.dtb \
ste-hrefprev60-stuib.dtb \
ste-hrefprev60-tvk.dtb \
ste-hrefv60plus-stuib.dtb \
Kind regards,
Erwan.
2025-04-02 3:08 AM - edited 2025-04-02 3:22 AM
The wiki does not mention the dts should be added to the Makefile:
https://wiki.st.com/stm32mpu/wiki/How_to_compile_the_device_tree_with_the_Developer_Package
make ARCH=arm st/stm32mp135f-stm32mp135f-dk-mx.dtb LOADADDR=0xC2000040 O="${OUTPUT_BUILD_DIR}"
This worked (also with a custom DT not in the Makefile) with ECO 5.0 but not with 6.0
2025-04-02 3:52 AM
As a quick test on OSTL v6, I tested to copy a dk dts and name it something such as stm32mp135f-dk-copy.dts.
The command you used worked on my side in this case.
Are you sure you have no syntax issue with your dts filename ?
Another test would be to add your specific DT in the Makefile and try a make dtbs.
Kind regards,
Erwan.
2025-04-02 4:22 AM - edited 2025-04-02 7:51 AM
Adding it to the Makefile worked.
Found the same issue with u-boot, the .dts file exists, is not in the Makefile, and does not build the dtb. in ECO 5.0 the DT was not added to makefile and the make did not fail
make DEVICE_TREE=$STM32MP_PROJECT DEBUG=1 LOG_LEVEL=LOG_LEVEL_INFO all/media/user/H3D2P1/Develop/STMICRO/STM_ECO_6.0.0/Developer-Package/u-boot-stm32mp-v2023.10-stm32mp-r1-r0/u-boot-stm32mp-v2023.10-stm32mp-r1/arch/arm/dts/stm32mp157a-board-mx-lcd.dts
Device Tree Source (arch/arm/dts/stm32mp157a-board-mx-lcd.dtb) is not correctly specified.
Please define 'CONFIG_DEFAULT_DEVICE_TREE'
or build with 'DEVICE_TREE=<device_tree>' argument
make[1]: *** [dts/Makefile:34: arch/arm/dts/stm32mp157a-board-mx-lcd.dtb] Error 1
make: *** [Makefile:1156: dts/dt.dtb] Error 2I do add the DEVICE_TREE option but still the error is reports
Used this for u-boot and the dtb was generated. Curious why DEVICE_TREE doesn't ?
CONFIG_DEFAULT_DEVICE_TREE=Device tree name
2025-04-02 7:50 AM
Correction: I did add the device tree files to the Makefile in ECO 5.0 to make it work. Suggest to add this in the WIKI to help others.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.