2025-11-10 11:24 PM - last edited on 2025-11-11 3:11 AM by Andrew Neil
I’m working on a custom STM32MP257DAK3 board.
In STM32CubeMX, I need both SDMMC1 (SD card) and SDMMC2 (eMMC) to be supported as possible boot devices.
When I check both:
SDMMC1 → Memory Boot Device
SDMMC2 → Memory Boot Device
The following error appears in IPs assignment rules:
Faulty state detected for SDMMC1, SDMMC2 : Only one Memory Boot Device can be assigned to TF-A simultaneously.
I understand that TF-A allows only one memory boot device at a time.
However, our hardware design supports dual boot options (either from eMMC or SD card). How can I fix this error?
Solved! Go to Solution.
2025-11-11 2:58 AM - edited 2025-11-11 3:45 AM
Hello @SullyNiu
"Faulty state detected for SDMMC1, SDMMC2: Only one Memory Boot Device can be assigned to TF-A simultaneously." is a non-blocking warning so you can still generate code and proceed.
THX
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-11-11 2:58 AM - edited 2025-11-11 3:45 AM
Hello @SullyNiu
"Faulty state detected for SDMMC1, SDMMC2: Only one Memory Boot Device can be assigned to TF-A simultaneously." is a non-blocking warning so you can still generate code and proceed.
THX
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.