2026-05-28 6:15 AM
Hello ST team,
I am working on STM32MP257F-EV1 with OpenSTLinux. I want to interface an external ADC from the M33 core using SPI3.
Target pins on 40-pin header:
PB1 = SPI3_NSS / manual CS PB7 = SPI3_SCK PB8 = SPI3_MOSI PB10 = SPI3_MISO
I created a custom Linux DTB for M33 SPI usage:
stm32mp257f-ev1-ca35tdcid-ostl-m33spi.dtb
In this DTB, I disabled SPI3 from A35/Linux:
spi@400c0000 {
compatible = "st,stm32mp25-spi";
reg = <0x400c0000 0x400>;
status = "disabled";
};I also changed /boot/mmc1_extlinux/extlinux.conf default entry to boot with this DTB:
DEFAULT OpenSTLinux-M33SPI
LABEL OpenSTLinux-M33SPI
KERNEL /Image.gz
FDT /stm32mp257f-ev1-ca35tdcid-ostl-m33spi.dtb
INITRD /st-image-resize-initrd
APPEND root=PARTUUID=491f6117-415d-4f53-88c9-6e0de54deac6 rootwait rw earlycon console=${console},${baudrate}After reboot, I confirmed A35/Linux SPI3 is disabled:
cat /sys/firmware/devicetree/base/soc@0/bus@42080000/spi@400c0000/status
Output:
disabled
Also Linux is not binding SPI3:
ls -l /sys/bus/platform/drivers/spi_stm32/ | grep 400c0000 ls /sys/bus/spi/devices/ ls /dev/spidev*
No SPI3/spidev is present.
M33 is running:
cat /sys/class/remoteproc/remoteproc0/name cat /sys/class/remoteproc/remoteproc0/state
Output:
m33 running
I tested the M33 firmware by blinking LED3, and LED3 blinks correctly, so the M33 firmware is running.
However, when I try to toggle PB1 from M33 as a simple GPIO output, there is no waveform on header pin 24. Because SPI3 also uses GPIOB pins PB7/PB8/PB10, SPI3 waveforms also do not appear.
My simple M33 GPIO test:
__HAL_RCC_GPIOB_CLK_ENABLE();
GPIO_InitTypeDef GPIO_InitStruct = {0};
GPIO_InitStruct.Pin = GPIO_PIN_1;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
while (1)
{
HAL_GPIO_TogglePin(GPIOB, GPIO_PIN_1);
HAL_Delay(500);
}LED3 still blinks in other test code, but PB1 does not toggle.
I checked OP-TEE patch/source and found that the STM32MP257 pinctrl GPIOB node appears as disabled:
pinctrl: pinctrl@44240000 {
compatible = "st,stm32mp257-pinctrl";
gpiob: gpio@44250000 {
gpio-controller;
#gpio-cells = <2>;
interrupt-controller;
#interrupt-cells = <2>;
#access-controller-cells = <1>;
reg = <0x10000 0x400>;
clocks = <&rcc CK_BUS_GPIOB>;
st,bank-name = "GPIOB";
status = "disabled";
};
};I also found RIF-related definitions:
STM32MP25_RIFSC_SPI3_ID = 24 STM32MP25_RIFSC_GPIOB_ID = 161 RCC_RIF_GPIOB = 91
SPI3 RIF entry in OP-TEE patch appears open/non-secure:
RIFPROT(STM32MP25_RIFSC_SPI3_ID, RIF_UNUSED, RIF_UNLOCK,
RIF_NSEC, RIF_NPRIV, RIF_UNUSED, RIF_SEM_DIS, RIF_CFDIS)My question:
For STM32MP257F-EV1, what is the correct way to assign GPIOB and SPI3 to the M33 core?
Specifically:
Is disabling spi@400c0000 in the Linux DTB enough to release SPI3 from A35?
How should GPIOB be enabled/assigned for M33 so that PB1/PB7/PB8/PB10 can be controlled by M33?
Should this be done in OP-TEE RIF device tree, TF-A RIF configuration, or Linux DT?
What exact RIF/GPIO configuration is required for:
GPIOB / PB1 / PB7 / PB8 / PB10
SPI3 peripheral
Is status = "disabled" for gpiob: gpio@44250000 expected in OP-TEE source, or should it be changed to "okay" for M33 GPIO usage?
I previously tried modifying TF-A/OP-TEE/RIF files, but the board stopped booting, so I want to know the correct safe method before changing boot-critical files again.
Current confirmed status:
A35/Linux SPI3 disabled: yes M33 remoteproc running: yes M33 LED blink works: yes M33 PB1 GPIO toggle: not working M33 SPI3 SCK/MOSI waveform: not working
Please suggest the correct device tree / RIF / OP-TEE configuration flow to give SPI3 and GPIOB access to M33 on STM32MP257F-EV1.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.