2025-11-10 7:21 PM - last edited on 2025-11-11 3:15 AM by Andrew Neil
I am experiencing a configuration validation warning related to RCC when generating code in STM32CubeMX version 6.15.0 for the STM32MP257DAK3 MPU. Although the code can be generated, CubeMX reports the following RCC warning during validation:
Main Config: These peripherals still have some not configured or wrong parameter values: [RCC]This warning appears even when the RCC configuration seems complete and valid.
Open STM32CubeMX v6.15.0
Create a new project for STM32MP257DAK3
Navigate to System Core → RCC
Set HSE to Crystal/Ceramic Resonator
Click GENERATE CODE
CubeMX displays the above warning during pre-generation configuration check
I've selected Pin Context Assignment from the dropdown menu, but it's empty.
2025-11-10 8:51 PM
Im also getting this prompt.
2025-11-10 11:18 PM - edited 2025-11-11 3:42 AM
Hello @SullyNiu @Andrew Neil
Your detailed explanation is much appreciated.
The issues have already been identified and escalated to the development team under internal ticket numbers 217338 (for the warning issue) and 216544 (for the Pin Context Assignment issue). They will be resolved as soon as possible.
THX
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.