cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX 6.15.0 released

Semer CHERNI
ST Employee

We are pleased to announce that the version 6.15.0 of STM32CubeMX is available.

What is new in 6.15.0:

  • Enhanced microprocessor support: Added the STM32MP21-A35-TD, STM32MP21-M33-TD, STM32MP25-M33-TD, and STM32MP23-M33-TD trusted domains for the STM32MP2 MPUs and their Arm® Cortex®-A35 and Cortex®-M33 processors.
  • Integrated the STARM-Clang toolchain:
    • The STMicroelectronics LLVM-based toolchain for Arm®, STARM-Clang, leverages Clang's modular architecture for faster compilation and enhanced support for modern language standards, expanding the build capabilities.
  • Build process enhancements:
    • Use of CMake for more efficient project compilation.
    • Removal of the -Wpedantic and -Wextra options from CMake GCC toolchain template to match the build results produced by STM32CubeIDE.
  • Updated the RIF feature implementation:
    • Integrated the RIF feature for STM32MP2 microprocessors with the STM32MP21-A35-TD, STM32MP21-M33-TD, STM32MP25-M33-TD, and STM32MP23-M33-TD trusted domains.
  • Updated software download management:
    • Added pause and resume functionalities to the software package download feature.
  • Updated the IAR Embedded Workbench® for Arm® toolchain (EWARM) support:
    • Added the support for STM32MP13xx microprocessors.
  • Updated the pin-to-pin compatibility:
    • Implemented the pinout compatibility for STM32MP2 microprocessors.
  • Added the wM-Bus middleware:
    • Implemented the wM-Bus PHY middleware for STM32WL33xx microcontrollers.
  • Updated the memory management tool (MMT):
    • Implemented memory management for the STM32U3.
  • Upgrade Azure RTOS [USBX ,LevelX ,FileX ,ThreadX]  6.2.0 to 6.4.0 for STM32WBA6​.
  • Upgraded the JxBrowser version to V8.5.0.

Main fixed issues in 6.15.0:

Refer to the STM32 microcontroller wiki at:
https://wiki.st.com/stm32mcu/wiki/STM32CubeMX_errata_6.15.x

Known problems and limitations in 6.15.0:

Refer to the STM32 microcontroller wiki at:

https://wiki.st.com/stm32mcu/wiki/STM32CubeMX_errata_6.15.x

How to get STM32CubeMX 6.15.0:

  • Under this link
  • Or update your current installation of STM32CubeMX using: Help > Check for Updates

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 REPLY 1
ymy
Associate II

很好奇,cubemx安装的库中为什么没有cubemx工程示例?

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.