STM32 MPUs Software development tools

Ask questions and find answers on STM32 microprocessors software development tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 505 Views
  • 0 replies
  • 0 kudos

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 392 Views
  • 0 replies
  • 0 kudos

STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! How to change the CPU clock frequency on STM32MP157F-EV1 board from 650MHz to 800MHz?

I noticed that even if I create a new project using STM32CubeMX IDE for STM32MP157F-EV1 board, in the clock configuration, the MPUSS_CK is 650MHz. In Linux, I can see the CPU frequency is 650MHz only. How can I clock the CPU to 800MHz as supported b...

New M4 project in cubeide has build button grayed out while running distribution package on STM32MP157c-DK2?

I am running the st-example-image-qt distribution package and am trying to use the M4 processor to feed sensor data to my UI. I can import the OpenAMP_TTY_echo example into stm32cubeide and debug it with my board fine. But now I am trying to make my ...

BSunw.1 by Associate III
  • 2242 Views
  • 2 replies
  • 0 kudos

CubeProgrammer shows that partition size is negative, fail to program using CubeProgrammer (kernel panic), but successful with raw SD card image using Win32DiskImager

Hi everyone,I have a problem using STM32CubeProgrammer (and CLI). They are both showing that my userfs partition have a size of -1162381824 bytes. That partition have size of 2.9GB. After programming with CubeProgrammer I have kernel panic, and I don...

0693W000007ZBa9QAG.png
NGajic by Associate III
  • 3160 Views
  • 6 replies
  • 0 kudos

Resolved! What is the layout of the .tsv file?

I'm updating a .tsv file, used by the CubeProgramer to program a STM32MP DK1. The file I'm looking at contains:#Opt Id Name Type IP Offset Binary - 0x01 fsbl1-boot Binary none 0x0 arm-trusted-firmware/tf-a-stm32mp157a-dk1-serialboot.stm32 - 0x03 ssbl...

MWors.1 by Associate II
  • 3060 Views
  • 3 replies
  • 0 kudos

How can i enable SPI5 on STM32MP157-DK1

Hi,Im working with STM32MP157A-DK1 board. Im working on the linux side, need to write C/C++ code for saving data into a SD card. I need to use SPI to get data from RF transceiver. I built linux and kernel as in this link:https://wiki.st.com/stm32mpu/...

MÇerçi by Associate III
  • 3376 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.