STM32 MPUs Software development tools

Ask questions and find answers on STM32 microprocessors software development tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 505 Views
  • 0 replies
  • 0 kudos

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 392 Views
  • 0 replies
  • 0 kudos

STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

STM32CubeIDE for OSX for MP1

Is it possible to use the CubeIDE on OSX for debugging firmware for STM32MP1?The interface is lacking some features and the debugging configuration is completely different.Also I can't manage to make it work.Here is what shows up when I launch Debug ...

0693W00000ANb7ZQAT.png
Sindel by Associate
  • 2580 Views
  • 3 replies
  • 0 kudos

Good afternoon. Using CubeMX, I created an empty project for the STM32MP157A-DK1 board. It compiles without errors. But when I try to start debugging in engineering mode, I get a message that there are too many breakpoints. When I try to start debugging i

Good afternoon. Using CubeMX, I created an empty project for the STM32MP157A-DK1 board. It compiles without errors. But when I try to start debugging in engineering mode, I get a message that there are too many breakpoints. When I try to start debugg...

Vlaty.1 by Senior
  • 2616 Views
  • 2 replies
  • 0 kudos

How to configure SDMMC Pin in STMCubeMx to make Board contain two SDMMC partitions both used for boot ?

Hello everyone, I'm configuring my STM32MP157C-DK2 Board pins and i want to make two SD Card partitions availabe. For the first one i chose the SDMMC1 and attributed it to PC10 pin for the second one do i need to choose SDMMC2 and to attribute it to ...

0693W00000AN55gQAD.png
FHami.1 by Associate
  • 2116 Views
  • 2 replies
  • 1 kudos

Resolved! Unable to boot from parallel NAND

Hello,I'm trying the NAND boot on our STM32MP157AAB3 custom board but until today I could't make the ROM code load the tf-a image from this memory.I'm yet able to boot from uSD (SDMMC1), eMMC (SDMMC2) and serial NOR (QUADSPI). For uSD I partitioned t...

RBors.1 by Associate II
  • 6530 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.